cancel
Showing results for 
Search instead for 
Did you mean: 

"project is part of hierarchical structure. Would you like to import entire project structure?"

RongShengWang
Associate III

Hi,

After CubeMX auto-code generation, CubeIDE shows message: " project XXX is part of hierarchical structure. Would you like to import entire project structure? Yes/NO?  "

if I choose "Yes", a sub-directory will be created inside my project which is not desirable. How to fix it?

Thanks,

Peter

2 REPLIES 2
Souhaib MAZHOUD
ST Employee

Hello @RongShengWang 

Ensure that the project is not generated inside another project and try to change the path of your project to another directory.

BR,

Souhaib

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

I had to check "Generate under root" checkbox in Project Manager". I did not, which wasted me 3 days to deal with many troubles caused by the simply clicking the checkbox. It should be defaulted to  "Generate under root"

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.