2019-10-28 6:18 AM
After generating code for a migrated project (from TrueStudio & CubeMX), I noticed a new file 'mx.scratch' in the project's root.
Is this a temp file that gets generated from other files or shall I take it under source control?
2019-10-28 10:22 AM
Yes such file is a temp file. If regular behavior you should see it only during CubeMX project generation process. If getting it by the end of the process most probably some unexpected issue happens in between.
2019-10-28 10:53 AM
I just reran code generation and 'mx.scratch' doesn't get deleted after it's done. But I don't get any error messages, and the produced code looks fine.
Is there a log somewhere that I can consult?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.