2023-11-09 2:52 AM
Board : STM32H745I - DISCO
Cubeide : v.1.13.2
TouchGFX : v4.22.1 Designer
STM32H745I - DISCO as it is dual core m4 and m7
1st i did build and debugging for m4 processor. It is successful.
2nly done with building for m7 processor.It is successful
But while debugging the m7 i am facing following issue ??????
please help me with this .
Error in final launch sequence:
Failed to execute MI command:
load C:\\TouchGFXProjects\\11092023\\STM32CubeIDE\\CM7\\Debug\\STM32H745I_DISCO_CM7.elf
Error message from debugger back end:
Load failed
Failed to execute MI command:
load C:\\TouchGFXProjects\\11092023\\STM32CubeIDE\\CM7\\Debug\\STM32H745I_DISCO_CM7.elf
Error message from debugger back end:
Load failed
Failed to execute MI command:
load C:\\TouchGFXProjects\\11092023\\STM32CubeIDE\\CM7\\Debug\\STM32H745I_DISCO_CM7.elf
Error message from debugger back end:
Load failed
Load failed
Solved! Go to Solution.
2023-11-10 10:50 AM - edited 2023-11-10 10:51 AM
Hello Chaitanya1997
Your case has been routed and your question will be further addressed through the online support system.
Kind Regards
Joe WILLIAMS
STMicro Support
2023-11-10 10:50 AM - edited 2023-11-10 10:51 AM
Hello Chaitanya1997
Your case has been routed and your question will be further addressed through the online support system.
Kind Regards
Joe WILLIAMS
STMicro Support
2025-03-07 2:10 AM
Hello @Joe WILLIAMS
I have the same issue than Chaitanya.
I have created a simple TouchGFX project for the board STM32H745I-DISCO. I can run the project from TouchGFX 4.25.0. I have imported the project to CubeIDE 1.17.0. I can compile both CM4 and CM7, I can run CM4 but when runing or debbuging CM7 the error Failed to execute MI command appears.
Please, do you know a solution for that?
Thank you.
2025-03-13 4:49 AM
Hello,
in my case the Mi error was because I needed to load an external loadar beacuse de QUADSPI flash.
In Run configurations -> Debugger.
Add external debugger -> C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\ExternalLoader\MT25TL01G_STM32H745I-DISCO.stldr
Regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.