2021-06-03 10:49 PM
I have recently bought Nucleo-G0B1RE Development board, When I power on, It worked perfectly I tested some programs on it and it worked very well. Then I ported my project on which I am working it executed sucessfully. But now I am facing weird problem, When I power on the nucleo board my none of the program is working !! In my project there is Monochrome graphics display used which is showing me the garbage, Even if I load the program from STM32Cube-IDE still it is not working and showing garbage on LCD. I doubt there is some reset problem on board. Please help me !!!
Thanks in advance
2021-06-15 4:45 AM
Hi @YVaid.1 ,
Try to make sure that the flash is erased using STM32CubeProgrammer then download your code again. Does it work this way?
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.