STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

GTK-Critical error on Linux (cubeide 1.6.1)

Hi, I recently tested cubeide 1.6.1 on latest Ubuntu 20.04 LTS and Debian 10.9.0 stable, both gave me GTK critical error when trying to launch configuration tool, both had issues with loading configuration menus (lists : sys, timers ect).​Im now inst...

oeliks by Senior
  • 1267 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F746, STM32CubeIDE

How to remember in STM32F746G-Disco uint32_t? Save after power off and recall when power is restored?Andrzej

Breakpoints do not work in CubeIde

I have 100pin STM32H750 VBT and CubeIde. Breakpoints don't work, "run to line" works. That is, the program newer stops at breakpoints. I read somewhere that ARM had a bug in some CPUs breakpoints. Is H750 one those. What are working CPUs. And yes, I ...

LMI2 by Lead
  • 1097 Views
  • 2 replies
  • 0 kudos

Trouble configuring the system clock for an STM32F303K8T6 for speeds higher than 16Mhz (using CubeMX and CubeIDE)

Hardware: My board is a custom board that has an STM32F303K8T6. It has an external 8Mhz crystal as well as a ferrite choke between VDDA and VDD, and other passive capacitors. Situation: I am trying to configure the system clock for 72mhz using Cube M...

AHatt.1 by Associate II
  • 16662 Views
  • 11 replies
  • 1 kudos

Doxygen with STM32CubeIDE

HelloI tried to use doxygen to a project folder from STM32CudeIDE but it does not generate the documentation. I also looked on how to use doxygen on eclipse but still no results.Is there a way to use doxygen or any other tool for generating documenta...

Avgerinos by Associate III
  • 5529 Views
  • 2 replies
  • 0 kudos

en.stm32cubeh7_v1-9-0\STM32Cube_FW_H7_V1.9.0\Projects\STM32H735G-DK\Demonstrations\Oscilloscope_SignalsGenerator\STM32CubeIDE

Oscilloscope_SignalsGenerator example Not Loading the Kit. i got the Error like Error in final launch sequence:Failed to execute MI command:load E:\\ST\\en.stm32cubeh7_v1-9-0\\STM32Cube_FW_H7_V1.9.0\\Projects\\STM32H735G-DK\\Demonstrations\\Oscillos...

senthil by Associate II
  • 6655 Views
  • 13 replies
  • 0 kudos

Resolved! Missing IRQ Handlers in .s file

Hey, I'm having issues with my Nucleo Board.I'm using an STM32F410RB Nucleo board. I started a new project as usual. When I go to the reference manual and to the interrupt vector table, I see that the USART 1 and USART 2 are on positions 37 and 38, r...

Drexter by Associate II
  • 10397 Views
  • 11 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.