2025-11-23 9:12 AM
Hi
Deleted all my first attempts, wanted a new clean start.
Then imported the "Templates" part of the ST provided "stm32cubec0-v1-4-0" examples.
But it won't run nor build (greyed out).
It says "The selection cannot be launched, and there are no recent lauches" (See attached)
I've been looking through to make one but with no luck.
The built in Help is not providing anything.
Solved! Go to Solution.
2025-11-24 9:06 AM
Did you set the toolchain to STM32CubeIDE? It is not the default.
If that's not it, attach an IOC you're having trouble with.
2025-11-23 10:47 AM
Create a new project for that chip in STM32CubeMX, generate code, open the project in STM32CubeIDE (via the popup) and compile/run.
Why are you trying to build the templates directory?
2025-11-24 8:25 AM
The attempt I posted above is only one of many -different- fruit less attempts.
Forgot to say I'm using V2.0.0 I understand there might be a problem with this version.
I've tried (actually wants to) make a clean new project by creating it with the now seperate CubeMX.
But when opening the CubeMX created project the IDE cannot compile nor build it.
I went to the templates to try and extract a working project out of it. But this also doesnt work.
2025-11-24 9:06 AM
Did you set the toolchain to STM32CubeIDE? It is not the default.
If that's not it, attach an IOC you're having trouble with.
2025-11-24 9:53 AM
Just gave it a new try. Lot of updating going on and new popups for accepting this and that.
ST changed something, though the Version still say 2.0.0
Even the ioc file in the IDE has a MX logo to it that by a click directs to MX.
Also the "open project" in the MX popup after "Generate code" works now, and opens the IDE.
I didn't know about the tool chain though. EWARN is default, which I understand noone really uses (?)
Above all the project also builds..
Thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.