2020-02-14 3:25 PM
Fresh installation, when I try to create a STM32 project a zip file with firmware is downloaded and unpacked, but I still get this error message:
"Code generation could not be done because necessary firmware package is missing. Not able to complete STM32Cube project."
I tried to download and unzip these files manually with no luck.
I have this issue on my both PCs with windows 10. Also the same thing happens regardless if I try to create a project for my Nucleo F030R8 or Nucleo L053R8.
2020-02-15 5:00 AM
STMCubeIDE > Help > Manage Embedded Software Packages shows the installed packages and offers options to add/remove new ones. Try that.
2020-02-15 5:16 AM
It didn't help. Creating a new project generates .ioc file but doesn't generate any code. I'm still getting this error message.
Also when I right-click on the .ioc file the option "generate code" is disabled
2020-02-17 11:19 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.