STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Missing firmware packages - can't create a project

Fresh installation, when I try to create a STM32 project a zip file with firmware is downloaded and unpacked, but I still get this error message:"Code generation could not be done because necessary firmware package is missing. Not able to complete ST...

KOlsz.1 by Associate II
  • 4590 Views
  • 3 replies
  • 0 kudos

Unable to update software packs

Hi,I am unable to update embedded software packages.To update I select "Manage embedded software packages" menu item. Packages manager window opens. I see "Check Firmware & Software. Download File updaters.zip" but progress bar stays at 0 bytes. Afte...

Dmitri by Associate II
  • 2335 Views
  • 3 replies
  • 0 kudos

Resolved! How do I uninstall STM32CubeIDE from macOS?

I would like to remove STM32CubeIDE (v1.2.0) from my Mac (os 10.14.6).Removing the IDE is straightforward, just drag the .app to the trash. But how do I remove the ST Link Server from my machine? The ST Link Server Installer doesn't specify where it ...

BFrau.1 by Associate
  • 4836 Views
  • 2 replies
  • 2 kudos

Bug in the debugger?

Not sure whether this is a GDB or Eclipse behavior, or "feature" of debug info created by gcc compiler...Debugger in CubeIDE and Atollic refuses to display pointers to volatile.For example: volatile char *ptr = some_func();It always says that such po...

Pavel A. by Super User
  • 2925 Views
  • 5 replies
  • 0 kudos

2 Warnings are generated from '.project' file with the references MCUEndUserDisabledTrustZoneProjectNature and MCURootProjectNature.

Hello, two warnings are generated from the '.project' file in STM32CubeIDE with the references MCUEndUserDisabledTrustZoneProjectNature and MCURootProjectNature The file was generated by STM32CubeMX. Unfortunately I did not find anything in the Inter...

Vincent1 by Associate
  • 1201 Views
  • 1 replies
  • 0 kudos

Building time

HelloI'm new to STM32 tools and i have installed STM32CubeIde. When i build a small project it takes over 1 min:1m.504ms. Is this due to a setting that i missed ?

Tte B.1 by Associate
  • 1468 Views
  • 2 replies
  • 0 kudos

I am developing a series of NUCLEO 144-based project around my house, the principle point being that they're Ethernet-connected. I'm using the NUCLEO F207ZG as a first device, and the STM32CubeIDE. Is that the right place to start?

I'm after some advice. I've just discovered the STM32 NUCLEO boards, and I've used many MPUs (Atmel, Microchip, TI) in the past. I'm a fairly experienced software developer, but this is strictly homer stuff.I've been trying to get the FreeRTOS/LWIP d...

AWard.1 by Associate
  • 1363 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.