2024-04-05 7:32 AM - last edited on 2025-02-07 12:22 AM by mƎALLEm
I have an H755ZL and so I downloaded CubeIDE and CubeMX to begin familiarizing myself. I am unable to install the cubeMX H7 package so I cannot generate any code for my MCU. In either CubeIDE or CubeMX when I go to "manage embedded software" nothing happens. I also cannot login as nothing happens when I click that either.
Solved! Go to Solution.
2024-04-06 11:22 AM
I think you were correct about Windows 7 support. I installed CubeIDE v1.10.0 and was able to open the Manage Embedded software screen. I can now select the board and it will generate a project but it doesn't seem to generate a CubeMX GUI. I installed CubeMX 5.6.0 and could generate a GUI and a project which would successfully open in CubeIDE. If I open that project the native MX GUI in CubeIDE renders and everything seems to be functional.
2024-04-09 4:11 AM - edited 2024-04-09 4:12 AM
Hello @christophersmith1618 ,
CubeIDE is only supported for Windows 10 and 11. So, using Windows 7 might affect the IDE functionality.
Thanks,
Rim.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.