2020-06-03 4:38 AM
I have found examples online searching under LWIP such as
// What is our current IP address?
//
ulIPAddr = lwIPLocalIPAddrGet();but I cannot find the function in the source code, or any other reference to reading my IP address. I would like to be able to read it regardless of whether I'm static or DHCP.
2020-06-03 9:19 AM
Okay, so with a little more hunting, I have
extern struct netif gnetif;
local_IP = gnetif.ip_addr.addr;
printf("IP %d.%d.%d.%d\n\r",(local_IP & 0xff), ((local_IP >> 8) & 0xff), ((local_IP >> 16) & 0xff), (local_IP >> 24));but if its DHCP, how do I know if the address is initialised?
2020-06-03 10:43 AM
To get IP address, use netif_ip4_addr() and ip4_addr_get_u32(). When using DHCP, use ip4_addr_isany_val() to determine if it's assigned. And take a look at lwIP's bunch of similar functions and macros.
2020-06-04 1:47 AM
Thats spot on - thank you!
More questions though, how do I read the subnet mask and MAC address also?
Finally can I set the host name manually as well? so if I look at the DHCP server reservations pool I can easily spot my device by name?
2020-06-05 3:54 AM
as an addition, how do I set the MAC Address?
I can find it hardcoded in ethernet.c which is fine if this was going to be a single unit, but if by some miracle it went into production then what is the mechanism to allow you to update it?
Host name I have figured out, I was just reading it wrong.
extern struct netif gnetif;
local_SubNet = ip4_addr_get_u32(netif_ip4_netmask(&gnetif));
local_Gateway = ip4_addr_get_u32(netif_ip4_gw(&gnetif));
2022-08-24 7:47 AM
Credit to GitHub copilot, which recommends me:
printf("IP address: %s\n", ip4addr_ntoa(&gnetif.ip_addr));
result:
IP address: 192.168.1.63
2022-08-27 5:51 PM
More correct version:
printf("IP address: %s\n", ip4addr_ntoa(netif_ip4_addr(&gnetif)));
2022-08-27 5:57 PM
> I can find it hardcoded in ethernet.c which is fine if this was going to be a single unit, but if by some miracle it went into production then what is the mechanism to allow you to update it?
Then you write a normal code, which updates the MAC address in both - the ETH registers and NETIF structure.
2022-08-28 4:17 PM
> Credit to GitHub copilot
Few years ago when I first seen the Cube, I hoped it would evolve in the direction of the Copilot: a tool that knows all the reference manuals, all errata, trained on all the examples, backed by a serious AI. Alas.
2022-09-04 12:58 PM
> trained on all the examples
Trained on mostly broken code...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.