2025-04-04 6:11 AM - last edited on 2025-04-04 6:31 AM by Andrew Neil
Hello everyone,
I recently installed the application on my computer running Ubuntu 24.04 LTS and created a new project, just like on Windows 10. When I try to build the automatically generated program, I encounter a very confusing error. Here is the error message displayed in the console:
Context:
- STM32CubeIDE version: 1.18.0
- Microcontroller used: STM32G070CBT6
- Project generated with STM32CubeMX
- Operating system: Ubuntu 24.04 LTS
Tests already performed:
- Cleaning and rebuilding the project (Project > Clean... then Build All).
- Resetting the index (Project > C/C++ Index > Rebuild).
- Checking the compiler in Project > Properties > C/C++ Build > Toolchain Editor. Modified the build command (Properties > C/C++ Build > Builder Settings), testing with and without make -j4.
- Re-import the project after deleting the workspace (File > Import > Existing Projects into Workspace).
- Checked the error logs (Window > Show View > Error Log).
- Updated STM32CubeIDE and firmware packs.
- I also tried running the application from a terminal, here is the message: 1 : `Invalid condition id : UX_CORESTACK_Condition cause : null`
Despite these steps, the error persists. Have you encountered this problem before or do you have other avenues to explore?
Thanks in advance for your help!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.