2022-12-05 10:06 PM
So in my linker filer I put
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000 , LENGTH = 4K
ROM (rx) : ORIGIN = 0x8000000 , LENGTH = 12K
DAT (r) : ORIGIN = 0x8000000+12K , LENGTH = 4K
}
/* Sections */
SECTIONS
{
/* The startup code into "ROM" Rom type memory */
.isr_vector :
{
. = ALIGN(4);
KEEP(*(.isr_vector)) /* Startup code */
. = ALIGN(4);
} >ROM
/* The program code and other data into "ROM" Rom type memory */
.text :
{
. = ALIGN(4);
*(.text) /* .text sections (code) */
*(.text*) /* .text* sections (code) */
*(.glue_7) /* glue arm to thumb code */
*(.glue_7t) /* glue thumb to arm code */
*(.eh_frame)
KEEP (*(.init))
KEEP (*(.fini))
. = ALIGN(4);
_etext = .; /* define a global symbols at end of code */
} >ROM
.udata :
{
. = ALIGN(4);
_udata = .;
*(.udata)
*(.udata*)
. = ALIGN(4);
KEEP (*(.udata))
} >DAT
}And then in the code const uint32_t data __attribute__ ((section(".udata"))) = 0x1234;
So how can I get the variable to be stored only in 0x8003000?
2022-12-05 10:22 PM
I think in C there is a coding way to hardcode the memory placement. In IAR the linker config file enablre creation of segments named and #pragma in the source code for the linker to place data where you unusually need them to be.
2022-12-05 11:21 PM
What you observe might actually be a correct behavior. First, check if the value appears in an init section or somewhere within the code. If it appears in the code - the compiler may optimize access to a constant by using its value instead of referring to it as data. In such a case, maybe using volatile specifier for it would remove the optimization.
2022-12-07 11:39 AM
Thanks for the replies. It works now, although I dont 100% know why. I think it did have to do with compiler optimization. I tried so much that I lost track of what it was in the end. :dizzy_face:
2022-12-07 12:22 PM
Perhaps look at what startup.s is doing with regard to the initialization, and the .MAP file as to where the linker places things. Might want to contrast behaviour there with/without optimization.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.