2021-01-27 4:14 PM
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 36K
BOOT_FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 12K
APP_FLASH (rx) : ORIGIN = 0x8003000, LENGTH = 52K
}
2021-01-27 5:54 PM
I was able to have two build projects, and able to share common files etc..which is great.
But at the end I get:
Error: Cannot find the specified linker script. Check the linker settings in the build configuration.
make[1]: *** [makefile:91: fail-specified-linker-script-missing] Error 2
make[1]: *** Waiting for unfinished jobs....
make: *** [makefile:52: all] Error 2
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.