2020-04-08 7:50 AM
I'm trying to run a simple blink sketch using a F031K6 nucleo board. I'm following the steps here - https://www.youtube.com/watch?v=hyZS2p1tW-g and when i get to the part where I go to 'debug as' I can't because it says 'none applicable'. I have the board connected via usb, I have installed a firmware update, drivers and the STlink server module.
how can I get this to work??
2020-04-08 2:34 PM
Install STLink Utility and try Target->Connect there.
Works?
JW
2020-04-09 1:54 AM
Hi, thanks for your reply.
Yes I can connect, it told me the first time to connect under reset mode, but after that it was all fine. Still nothing happens with STMcubeIDE
2020-04-09 2:21 AM
I don't use CubeIDE so I don't know, but maybe you should try to set it to connect under reset, too.
Although, connect under reset shouldn't be needed for a new device - try to chip-erase it in the STLink Utility, then disconnect, reconnect - still requires connect under reset?
JW
2020-04-09 2:52 AM
i erased the chip but it still requires connect under reset.
could it be because i used the firmware update? im really confused over this
2020-04-09 3:04 AM
No I think it is generally because the debugger implementation here is very fragile. Use better tools.
Watch that your code/settings don't disable the debug interface, reconfigure the debug pins, or power down the pins/logic you need to be working.
2020-04-09 3:17 AM
thanks, but I am a completely new user. I have experience with 8 bit avrs, but nothing with STM chips. What do you mean by 'better tools'?
All I have done is generated the code to setup the in/outs, nothing else
2020-04-09 5:05 AM
> All I have done is generated the code to setup the in/outs, nothing else
Which in/outs, namely?
JW
2020-04-09 5:08 AM
Hi! I got it working, not sure what I did but the the options just appeared suddenly. All seems to be working fine now, thanks for your help
2023-12-14 7:20 PM
I have encountered the same problem, can you tell me how you solved it?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.