2020-12-01 1:08 AM
Hi,
I'm working on Stm32CUBE IDE with STM32LO71RB. I would like to write a version number when I am flashing my device at EEPROM Flash memory address 0x08080000. I've tried HAL_FLASH_Program(), but I have to execute it at each reset. I would like to do the same as an One-time programmable memory but it's not availlable in STM32 cortex M0+.
Is there any other possibilities to write directly in EEPROM memory?
best,
Solved! Go to Solution.
2020-12-01 3:39 AM
You can only write flash once unless you erase i n between. But erase erases full sectors, that's the difference to EEPROM
2020-12-01 1:35 AM
Look for EEPROM emulation. B.t.w. I think 0x08080000 is no good place, it is in the middle of the code space. Move it to top of flash.
2020-12-01 3:02 AM
Thank you for youyr answer, I already use HAL_flash and Hal_flash-ex for the eeprom emulation. Thanks for the tips but I did'nt find my answer in the doc or maybe is not the good formulation.
I know that in microchiop environment it is possible to write directly in assembly to the memory at the flashing moment.
asm("\
PSECT absdata,delta=2,abs\n\
ORG 1000h\n\
dw 1111h\n\
"); Currently, I've have that:
void main (void)
{
//HAL _init ...
HAL_FLASH_Unlock();
if(HAL_FLASH_Program(FLASH_TYPEPROGRAM_WORD, ADDR , data) != HAL_OK)
Error_Handler();
HAL_FLASH_Lock();
while(1){
}
}For me, if I restart the code, the write EEPROM operation will be execute another time and the variable "data" is stored twice, in the Flash Code and in the EEPROM.
I would like to find a way to execute it only once.
Tel me if my reasoning doesn't work?
2020-12-01 3:39 AM
You can only write flash once unless you erase i n between. But erase erases full sectors, that's the difference to EEPROM
2020-12-01 6:44 AM
ok thanks, I understand it better.
So if y want to write to the flash, I have to modify my linker and use __atribute__ to allocate memory to my data like it said on this topic ?
https://stackoverflow.com/questions/28503808/allocating-memory-in-flash-for-user-data-stm32f4-hal
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.