cancel
Showing results for 
Search instead for 
Did you mean: 

How to use CMSIS-DSP now that there are no precompiled libs in the firmware packs

theRat
Associate II

I am using STM32CubeIDE 1.13.0 with the latest firmware packs targeting a STM32H563 and need to include the CMSIS-DSP library.
All of the forum posts/youtube videos/howto's etc say to copy a precompiled library file from the firmware repository to your project and then reference it.  The problem is that the current firmware repositories no longer contain pre-compiled libraries, only source code.  So can someone provide an updated set of instructions describing how to use the DSP code.

Cheers
Simon

11 REPLIES 11
CKugl.1
Senior II

I've gone through this process a few times before and it's always a huge hassle. Here's how I got it done today:

  1. mkdir CMSIS-DSP
  2. cd CMSIS-DSP
  3. git clone git@github.com:ARM-software/CMSIS-DSP.git
  4. git clone git@github.com:ARM-software/CMSIS_6.git
  5. Create a CMakeLists.txt like the following:

 

cmake_minimum_required(VERSION 3.16)
set(CMAKE_TOOLCHAIN_FILE ${CMAKE_CURRENT_SOURCE_DIR}/toolchain.cmake)

set(HOME $ENV{HOME})
set(CMSISDSP ${CMAKE_CURRENT_SOURCE_DIR}/CMSIS-DSP)
set(CMSISCORE ${CMAKE_CURRENT_SOURCE_DIR}/CMSIS_6/CMSIS/Core)

add_compile_options(
    -mcpu=cortex-m4
    -std=gnu11
    -ffunction-sections
    -fdata-sections
    #--specs=nano.specs
    -mfpu=fpv4-sp-d16
    -mfloat-abi=hard
    -mthumb
    
    -Wsign-compare
    -Wdouble-promotion
    -Ofast -ffast-math
    -DNDEBUG
    -Wall -Wextra  -Werror
    -fshort-enums 
    #-fshort-wchar
    )
add_link_options(
    -mfloat-abi=hard    
    -mcpu=cortex-m4
    -Wl,--gc-sections
    -static
    -mfpu=fpv4-sp-d16
    -mthumb
    )
## Define the project
project (cmsis-dsp)

add_subdirectory(${CMSISDSP}/Source bin_dsp)

 

(You will probably have to adjust some options for your particular STM32 chip. Look in your project's Properties / C/C++ Build Settings / MCU GCC Compiler / All options and MCU G++ Linker / All options to see what STM32CubeIDE is using.)

  • Create a toolchain.cmake file like the following:

 

# the name of the target operating system
set(CMAKE_SYSTEM_NAME Generic)
set(CMAKE_SYSTEM_PROCESSOR arm)
set(CMAKE_CROSSCOMPILING 1)
set(CMAKE_C_COMPILER arm-none-eabi-gcc)
set(CMAKE_CXX_COMPILER arm-none-eabi-g++)
set(CMAKE_ASM_COMPILER arm-none-eabi-gcc)
set(CMAKE_OBJCOPY arm-none-eabi-objcopy)
set(CMAKE_SIZE_UTIL arm-none-eabi-size)
set(CMAKE_C_GDB arm-none-eabi-gdb-py)
set(CMAKE_AR arm-none-eabi-gcc-ar)
set(CMAKE_RANLIB arm-none-eabi-gcc-ranlib)

set(CMAKE_EXE_LINKER_FLAGS "--specs=nosys.specs" CACHE INTERNAL "")

# This should be safe to set for a bare-metal cross-compiler
set(CMAKE_FIND_ROOT_PATH_MODE_PROGRAM NEVER)
set(CMAKE_FIND_ROOT_PATH_MODE_LIBRARY ONLY)
set(CMAKE_FIND_ROOT_PATH_MODE_INCLUDE ONLY)
set(CMAKE_FIND_ROOT_PATH_MODE_PACKAGE ONLY)

 

  • mkdir build
  • cd build
  • cmake ..
  • make -j4

This should produce a libCMSISDSP.a file in CMSIS-DSP/build/bin_dsp.

Now, in STM32CubeIDE, you can

  1. Go to your project's Properties / C/C++ Build Settings / MCU G++ Linker / Libraries
  2. Under Libraries (-l), add CMSISDSP
  3. Under Library Search Path (-L), add the full path to the directory containing libCMSISDSP.a
  4. Go to your project's Properties / C/C++ Build Settings / MCU GCC Compiler / Include paths and add the full path to CMSIS-DSP/CMSIS-DSP/Include/

 

Thanks a lot CKugl.1 . Your answer made my day :)

 

I provide below my feedback on this matter, in case it can help any one out there in a similar situation:

 

I come from the STM32F4 family and have been using CMSIS-DSP precompiled libraries for STM32F4 family for a while now.

 

Recently I upgraded to the new STM32H5 family, for which no precompiled CMSIS-DSP libraries are availalble. After some (or rather a lot of) search online and following the official instructions of CMSIS-DSP github I managed to add the source files to the project and compile the libraries from source within STM32CubeIDE. I followed my own steps, but they were rather similar to the ones detailed in this ST post by the ST team .

 

However, after testing the libraries for a while I observed a really strange behaviour in some of the functions of the library, mostly some functions related to FFT transformations, when compiling the project  with the Optimization option for speed , as this was the recommended option instructed in CMSIS-DSP github:

 

-Ofast

 

Indeed, with this option I had a gain in computation speed of approximately 60%, but the results of FFT operations , multiplications of complex vectors, etc. were just not right!!

I was then trying to find a way to precompile the CMSIS-DSP libraries externally and ended up in your reply CKugl.1 .

 

For me this is definately the way to go and should be the recommended method for integrating this libraries into the STM32 MCUs. Now I can have the CMSIS-DSP libraries compiled for speed optimization externally and leave the project with Optimization option "None". So now the code is working accurate as a clock and I am also saving processing time. So thanks a lot for this!

 

Cheers,

Diego

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.