2024-08-20 5:40 PM
Hello,
I am encountering an issue while debugging a project using STM32CubeIDE. The problem arises when I start the debugging process. Below is the output from the console:
Open On-Chip Debugger 0.12.0+dev-00597-ga5a21219f (2024-06-03-11:04)
Licensed under GNU GPL v2
For bug reports, read
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : STLINK V2J45S7 (API v2) VID:PID 0483:3748
Info : Target voltage: 3.198949
Info : clock speed 1800 kHz
Info : stlink_dap_op_connect(connect)
Info : SWD DPIDR 0x1ba01477
Info : [STM32F103C8Tx.cpu] Cortex-M3 r1p1 processor detected
Info : [STM32F103C8Tx.cpu] target has 6 breakpoints, 4 watchpoints
Info : [STM32F103C8Tx.cpu] Examination succeed
Info : starting gdb server for STM32F103C8Tx.cpu on 3333
Info : Listening on port 3333 for gdb connections
Info : accepting 'gdb' connection on tcp/3333
Info : device id = 0x20036410
Info : flash size = 64 KiB
undefined debug reason 8 (UNDEFINED) - target needs reset
Info : accepting 'gdb' connection on tcp/3333
undefined debug reason 8 (UNDEFINED) - target needs reset
[STM32F103C8Tx.cpu] halted due to breakpoint, current mode: Thread
xPSR: 0x01000000 pc: 0x080004a8 msp: 0x20005000
[STM32F103C8Tx.cpu] halted due to breakpoint, current mode: Thread
xPSR: 0x01000000 pc: 0x080004a8 msp: 0x20005000
Info : dropped 'gdb' connection
[STM32F103C8Tx.cpu] halted due to debug-request, current mode: Thread
xPSR: 0x21000000 pc: 0x080005e0 msp: 0x20004fd8
shutdown command invoked
Info : dropped 'gdb' connection
It seems to repeatedly halt due to a breakpoint, and there’s an "undefined debug reason 8 (UNDEFINED)" error message indicating that the target needs a reset. The debugger appears to lose the connection after this.
Could please provide guidance on how to resolve this issue or any suggestions on what might be causing it?
Thank you.
2024-08-21 5:37 AM
> STM32F103C8Tx
Is this a genuine ST chip or a counterfeit product? The vast majority of these chips are not genuine. Some work, some misbehave to various degrees.
Is your programmer genuine? Same caveats apply. STM32CubeIDE does not work well with counterfeit programmers.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.