2024-11-24 10:04 AM
Hello together,
I have installed the latest Linux mint at me and the latest STM32CubeIDE.
My board is STM32L010 Value Line Nucleo-64 (MCU: STM32L010RBT6 64 Pins).
I have encountered again the problem with the GDB version.
I cannot start the debug mode or run the compiled code.
I received this error message.
"Could not determine GDB version using command: arm-none-eabi-gdb --version
arm-none-eabi-gdb: error while loading shared libraries: libncurses.so.5: cannot open shared object file: No such file or director"
I have tried to use the previous solution to install the ncurses5. "sudo apt-get install libncurses5 libncurses5:i386".
It said the package is not found.
Can anyone please provide me any solution here?
Thank you!
2024-11-24 1:27 PM
Someone could already build the gdb without dependency on any libcurses at all.
2024-11-25 11:35 AM
I think it is required in STM32CubeIDE. If I configure to use ST Link GDB debugger.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.