2020-03-19 7:17 AM
Hello,
I use STMCube IDE v1.3.0 Build: 5720_20200220_1053 (UTC)
When building, the include path are not updated with the include path properties.
I notice this mis-alignement is caused in the cproject :
include path are correct here :
<option IS_BUILTIN_EMPTY="false" IS_VALUE_EMPTY="false" id="com.st.stm32cube.ide.mcu.gnu.managedbuild.tool.c.compiler.option.includepaths.26262030" name="Include paths (-I)" superClass="com.st.stm32cube.ide.mcu.gnu.managedbuild.tool.c.compiler.option.includepaths" useByScannerDiscovery="false" valueType="includePath">
<listOptionValue builtIn="false" value="C:/Users/fto/STM32Cube/Repository/STM32Cube_FW_L4_V1.15.1/Drivers/CMSIS/Include"/>
<listOptionValue builtIn="false" value="C:/Users/fto/STM32Cube/Repository/STM32Cube_FW_L4_V1.15.1/Drivers/STM32L4xx_HAL_Driver/Inc/Legacy"/>
<listOptionValue builtIn="false" value="C:/Users/fto/STM32Cube/Repository/STM32Cube_FW_L4_V1.15.1/Drivers/STM32L4xx_HAL_Driver/Inc"/>
<listOptionValue builtIn="false" value="C:/Users/fto/STM32Cube/Repository/STM32Cube_FW_L4_V1.15.1/Drivers/CMSIS/Device/ST/STM32L4xx/Include"/>
<listOptionValue builtIn="false" value="../Core/Inc"/>
<listOptionValue builtIn="false" value="../Core/Inc/Acc"/>
<listOptionValue builtIn="false" value="../Core/Inc/AlgoItf"/>
<listOptionValue builtIn="false" value="../Core/Inc/Bluetooth"/>
<listOptionValue builtIn="false" value="../Core/Inc/Button"/>
<listOptionValue builtIn="false" value="../Core/Inc/Flash"/>
<listOptionValue builtIn="false" value="../Core/Inc/ISL"/>
<listOptionValue builtIn="false" value="../Core/Inc/Ouput"/>
<listOptionValue builtIn="false" value="../Core/Inc/PwrMgmt"/>
<listOptionValue builtIn="false" value="../Core/Drivers/CMSIS/Device/ST/STM32L4xx/Include"/>
<listOptionValue builtIn="false" value="../Core/Drivers/CMSIS/Include"/>
<listOptionValue builtIn="false" value="../Core/Librairies/STM32L4xx_HAL_Driver/stm32l443xx/V1.11.0/Inc/"/>
<listOptionValue builtIn="false" value="../Core/Librairies/STM32L4xx_HAL_Driver/stm32l443xx/V1.11.0/Inc/Legacy"/>
<listOptionValue builtIn="false" value="../Core/Librairies/Bluetopia/include"/>
<listOptionValue builtIn="false" value="../Core/Librairies/Bluetopia/btpskrnl"/>
<listOptionValue builtIn="false" value="../Core/Librairies/Bluetopia/btpsvend"/>
<listOptionValue builtIn="false" value="../Core/Librairies/Bluetopia/btvs"/>
<listOptionValue builtIn="false" value="../Core/Librairies/Bluetopia/hcitrans.dma"/>
<listOptionValue builtIn="false" value="../Core/Librairies/Bluetopia/profiles/AUDIO/include"/>
<listOptionValue builtIn="false" value="../Core/Librairies/Bluetopia/profiles/A2DP/include"/>
<listOptionValue builtIn="false" value="../Core/Librairies/Bluetopia/profiles/AVCTP/include"/>
<listOptionValue builtIn="false" value="../Core/Librairies/Bluetopia/profiles/AVRCP/include"/>
<listOptionValue builtIn="false" value="../Core/Librairies/Bluetopia/profiles/GAVD/include"/>
<listOptionValue builtIn="false" value="../Core/Librairies/Bluetopia/profiles/HDSET/include"/>
<listOptionValue builtIn="false" value="../Core/Librairies/Bluetopia/profiles/HFRE_16/include"/>
</option>
But are not aligned there :
<tool id="com.st.stm32cube.ide.mcu.gnu.managedbuild.tool.c.compiler.1351960159" name="MCU GCC Compiler" superClass="com.st.stm32cube.ide.mcu.gnu.managedbuild.tool.c.compiler.1486773777">
<option IS_BUILTIN_EMPTY="false" IS_VALUE_EMPTY="false" id="com.st.stm32cube.ide.mcu.gnu.managedbuild.tool.c.compiler.option.includepaths.175873836" name="Include paths (-I)" superClass="com.st.stm32cube.ide.mcu.gnu.managedbuild.tool.c.compiler.option.includepaths" useByScannerDiscovery="false" valueType="includePath">
<listOptionValue builtIn="false" value="C:/Users/fto/STM32Cube/Repository/STM32Cube_FW_L4_V1.15.1/Drivers/CMSIS/Include"/>
<listOptionValue builtIn="false" value="C:/Users/fto/STM32Cube/Repository/STM32Cube_FW_L4_V1.15.1/Drivers/STM32L4xx_HAL_Driver/Inc/Legacy"/>
<listOptionValue builtIn="false" value="C:/Users/fto/STM32Cube/Repository/STM32Cube_FW_L4_V1.15.1/Drivers/STM32L4xx_HAL_Driver/Inc"/>
<listOptionValue builtIn="false" value="C:/Users/fto/STM32Cube/Repository/STM32Cube_FW_L4_V1.15.1/Drivers/CMSIS/Device/ST/STM32L4xx/Include"/>
<listOptionValue builtIn="false" value="C:/Travail/Projets/ComCom/EclipseWorkspaces/STMCube_TPGE/ComCom/Core/Inc/"/>
<listOptionValue builtIn="false" value="C:/Travail/Projets/ComCom/EclipseWorkspaces/STMCube_TPGE/ComCom/Core/Inc/Acc"/>
<listOptionValue builtIn="false" value="C:/Travail/Projets/ComCom/EclipseWorkspaces/STMCube_TPGE/ComCom/Core/Inc/AlgoItf"/>
<listOptionValue builtIn="false" value="C:/Travail/Projets/ComCom/EclipseWorkspaces/STMCube_TPGE/ComCom/Core/Inc/Bluetooth"/>
<listOptionValue builtIn="false" value="C:/Travail/Projets/ComCom/EclipseWorkspaces/STMCube_TPGE/ComCom/Core/Inc/Button"/>
<listOptionValue builtIn="false" value="C:/Travail/Projets/ComCom/EclipseWorkspaces/STMCube_TPGE/ComCom/Core/Inc/Flash"/>
<listOptionValue builtIn="false" value="C:/Travail/Projets/ComCom/EclipseWorkspaces/STMCube_TPGE/ComCom/Core/Inc/ISL"/>
<listOptionValue builtIn="false" value="C:/Travail/Projets/ComCom/EclipseWorkspaces/STMCube_TPGE/ComCom/Core/Inc/Output"/>
<listOptionValue builtIn="false" value="C:/Travail/Projets/ComCom/EclipseWorkspaces/STMCube_TPGE/ComCom/Core/Inc/PwrMgmt"/>
</option>
2020-03-19 1:22 PM
Generally, if you clean and rebuild a project, everything gets updated.
2020-03-19 3:29 PM
Thank you for your answer, but this is not the case. When building what I can see in the log, the include path are not what I set in the property window of STMCubeIDE. (Under Properties -> C/C++ Build -> settings -> Tool Setting tab -> MCU GCC compiler -> Include Path).
In the logs, following arm-none-eabi-gcc command, the arguments after -I are not what I set.
From what I see, the cproject contains 2 sections for the include path. This is was I wrote before.
The first section correspond to what I set in the window properties.
The second section correspond to what is used when I compile. It contains the resolved paths. But the resolved paths does not correspond to the relative path.
There is a mismatch somewhere cause by STMCubeIDE
2020-03-23 2:28 PM
Please could you share your full .cproject ?
I may only based on your limited current sharing advice to take care about build configuration you're relying on. Possibly doing some include path settings for one but building a second ...
I'm thinking to such because according your extract both are not related to same build configuration because IDs are not same here after:
+ id="com.st.stm32cube.ide.mcu.gnu.managedbuild.tool.c.compiler.option.includepaths.175873836"
+ id="com.st.stm32cube.ide.mcu.gnu.managedbuild.tool.c.compiler.option.includepaths.26262030"
2020-03-24 8:05 AM
2020-03-25 7:54 AM
Indeed there is something odd with the folderInfo xml tag.
It is like I have a folder which is not part of the project and have a different configuration.
How can I align this folder with all the project ?
2020-03-25 8:21 AM
I found the problem.
I don't why but one of my folder had a different configuration than the project.
To fix this, I right click on the folder with the problem, then select Ressources configuration then click Reset to default.
@Cartu38 OpenDev Thank you for your answer which lead me to the path of solving.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.