2019-11-30 8:13 PM
Hello,
I am generating code using STM32CubeIDE ,but when i start to debug getting error like-
"STMicroelectronics ST-LINK GDB server. Version 5.2.3
Copyright (c) 2019, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
Waiting for debugger connection...
Debugger connected
Debugger connection lost.
Shutting down..."
I am using latest version of st-link USB driver(en.stsw link009).Also i am using USB to TTL converter.Initially everything working very well,near about ten code executed successfully.But now facing the above error.So how can i solve it?
Thanks in advance.
2020-03-01 8:27 AM
Currently having the same issue - only difference is ST-LINK GDB server Version 5.5.0. Did you ever find a solution?
2020-03-01 3:23 PM
This happens to me quite frequently with a Nucleo board, and is usually fixed by unplugging then plugging back in the usb cable of your device. It's extremely frustrating that it is this unstable, but many other users seem to report similar things.
2020-03-06 6:14 AM
Same problem here with STM32g071 nucleo! any suggestions?
2020-04-09 3:50 AM
Try to debug with the ST-LINK using a different project. It should work (worked for me atleast). Then again try with the original project.
2020-12-31 11:55 AM
I have the same issues:
Debugger connection lost.
Shutting down...
I have created a new post for this.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.