2023-04-26 7:43 AM
I start the installation of STM32CubeIde on Debian 12, but it is impossible to continue the installation because it needs libpython2.7 and I have python3 installed on system. I can't downgrade the system.
How can I do?
Thank you
2023-12-02 12:03 PM
This way worked for me too, I'm using debian SID (trixie).
Many thanks!
2024-06-20 7:52 AM
I tryed the same thing on 20.6.2024. But it is still the same. I run into a dependency hell!!!!!!!!!!!!!
Would someone from STM take care of this. Just install stmcupeide on a new setup Debian!!!
2024-08-30 4:28 AM - edited 2024-08-30 4:40 AM
For ci, I managed to install python2.7 following https://www.fadedbee.com/2024/01/18/installing-python2-on-debian-12-bookworm/ .
After that I needed to add a tool from testing (to get a recent version), which broke the setup.sh script because of this line in it:
if [ $distro = "debian" -a $distro_version = "8" ] ; then
While the reason obvious, running shellcheck will help reveal other potential issues (and some false positives) to the maintainers of the install script. My workaround was to write appropriate version information to /etc/os-release so that $distro_version is not empty which was breaking the test expression - probably because I am using "testing".
After adding `mime-support shared-mime-info libgtk-3-0` to the packages I installed before starting the setup.sh script, it all works out again.
To build on debian from the cli, I use something like this:
bash -c "pwd ; $${STM32CUBEIDE} --launcher.suppressErrors -nosplash -application org
.eclipse.cdt.managedbuilder.core.headlessbuild -data '/workspace' -import . -cleanBuild PROJECT/Release"
As I use PREBUILD and POSTBUILD steps and the integrated GNU Make, I made those settings compatible with both Windows and LInux (which is copied as is in the generated makefile):
$(if $(findstring mingw,$(subst MINGW,mingw,$(MAKE_HOST))),..\PREBUILD.BAT,../PREBUILD.sh)
2024-10-23 10:21 PM
You can extract the packages from the shell script with the option --target <dirname>
Then you can use dpkg -i to install most of the packages and fix the dependencies the main package needs to forced the installation as it thinks it needs python 2.7.
sudo ./st-stm32cubeide_1.16.1_22882_20240916_0822_amd64.deb_bundle.sh --target ./stmPackages
sudo dpkg --force-depends -i st-stm32cubeide-1.16.1-22882-20240916-0822_amd64.deb
It seems to work, I would not be surprised it it completely works as python is mostly backward comptable maybe some python packages will be broken.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.