2019-10-09 6:24 AM
Can't find any drop down menu or other pointer to this functionality in STM32CubeIDE v. 1.0.2. My stm32 device - STM32 F429ZI - Nucleo. Please, help me to solve the problem?
2019-10-09 10:04 PM
Do you want to flash the chip without a USB connection?
Or do you want your program to run after flashing, and after disconnecting the USB cable?
2019-10-10 12:09 AM
I want my program (after building in STM32CubeIde v. 1.0.2) to run AFTER disconnecting the USB cable.
2019-10-10 12:21 AM
2019-10-10 12:26 AM
Do you mean that since i have run once my program in debug mode on device, it apears in flash and after that the one thing i need to do is to connect it to external power supply and disconnect from USB?
2019-10-10 12:29 AM
2019-10-10 1:04 AM
Unfortunately, after i disconnect USB and leave only power supply, my stm device turns off :(
2019-10-10 7:09 AM
2019-10-10 7:27 AM
What version of firmware is running on the ST-LINK? What power supply jumpers are set? You could try removing SB111
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.