2024-01-04 3:06 AM - edited 2024-01-04 3:14 AM
During the debugging, I noticed HAL_GetTick() freezes, I mean uwTick does not update anymore and holds the same value.
This issue is happening while the TIM15_IRQHandler is called and executes a function responsible for reading from an SPI communication, it is shown below:
uint8_t canSpi_readAdresss(spi_SlaveInterface* spi, uint8_t adress, uint8_t* rxData, uint8_t rxBytes)
{
uint8_t rxArray[2 + rxBytes];
uint64_t timeout = HAL_GetTick() + 5;
while (timeout > HAL_GetTick())
{
if (spi->master->activSlave == NULL)
{
uint8_t msgData[2];
msgData[0] = 0b00000011; // read
msgData[1] = adress;
if (spi_TransmitReceive_(spi, msgData, 2, rxArray, rxBytes) == 0)
{
for (uint8_t i = 0; i < rxBytes; ++i)
{
rxData[i] = rxArray[2 + i];
}
return 0;
}
else
{
//rxData = 0;
}
}
}
return 0xff;
}
The HAL_GetTick() holds the same value, therefore the execution gets stuck in the while-loop. It can happen just after the debugging starts or any time later.
The Tick priority uwTickPrio is 0 "zero", always.
Below is an image from the code execution shown in Parallel Stacks:
As it is the first time I am facing this kind of issue, I am a bit confused about what might be causing it.
Any help would be highly appreciated.
The settings are:
MCU: STM32F303VE
Microsoft Visual Studio Professional 2019 - Version 16.11.30
VisualGDB Version 5.6R9
Solved! Go to Solution.
2024-01-04 6:23 AM
uint8_t NVIC_IRQChannelPreemptionPriority = 1; uint8_t NVIC_IRQChannelSubPriority = 1;
The typical configuration has 4 bits for preemption priority and 0 for subpriority. Have you changed the NVIC priority grouping?
If you show the contents of the relevant NVIC registers, surely the issue will be apparent.
2024-01-04 3:53 AM
Timer tick prio must be higher (lower number) than TIM15_IRQHandler prio to increment the tick value within the handler.
hth
KnarfB
2024-01-04 4:58 AM - edited 2024-01-04 4:59 AM
Hi @KnarfB , thanks for the answer.
I forgot to mention, the uwTickPrio is lower than TIM15_IRQHandler, which is 1
Here is the function to set the TIM15
void EnableTimerInterruptTim15()
{
uint8_t NVIC_IRQChannel = TIM15_IRQn;
uint8_t NVIC_IRQChannelPreemptionPriority = 1;
uint8_t NVIC_IRQChannelSubPriority = 1;
FunctionalState NVIC_IRQChannelCmd = ENABLE;
uint32_t tmppriority = 0x00, tmppre = 0x00, tmpsub = 0x0F;
/* Check the parameters */
assert_param(IS_FUNCTIONAL_STATE(NVIC_IRQChannelCmd));
assert_param(IS_NVIC_PREEMPTION_PRIORITY(NVIC_IRQChannelPreemptionPriority));
assert_param(IS_NVIC_SUB_PRIORITY(> NVIC_IRQChannelSubPriority));
if (NVIC_IRQChannelCmd != DISABLE)
{
/* Compute the Corresponding IRQ Priority --------------------------------*/
tmppriority = (0x700 - ((SCB->AIRCR) & (uint32_t)0x700)) >> 0x08;
tmppre = (0x4 - tmppriority);
tmpsub = tmpsub >> tmppriority;
tmppriority = (uint32_t)NVIC_IRQChannelPreemptionPriority << tmppre;
tmppriority |= NVIC_IRQChannelSubPriority & tmpsub;
tmppriority = tmppriority << 0x04;
NVIC->IP[NVIC_IRQChannel] = tmppriority;
/* Enable the Selected IRQ Channels --------------------------------------*/
NVIC->ISER[NVIC_IRQChannel >> 0x05] =
(uint32_t)0x01 << (NVIC_IRQChannel & (uint8_t)0x1F);
}
else
{
/* Disable the Selected IRQ Channels -------------------------------------*/
NVIC->ICER[NVIC_IRQChannel >> 0x05] =
(uint32_t)0x01 << (NVIC_IRQChannel & (uint8_t)0x1F);
}
}
Thank you!
2024-01-04 6:23 AM
uint8_t NVIC_IRQChannelPreemptionPriority = 1; uint8_t NVIC_IRQChannelSubPriority = 1;
The typical configuration has 4 bits for preemption priority and 0 for subpriority. Have you changed the NVIC priority grouping?
If you show the contents of the relevant NVIC registers, surely the issue will be apparent.
2024-01-04 6:37 AM
In addidtion to @TDK :
compare your code to (or better use directly) CMSIS NVIC functions.
See https://arm-software.github.io/CMSIS_5/Core/html/group__NVIC__gr.html
and your local CMSIS installation like Drivers/CMSIS/Core/Include/core_cm*.h
hth
KnarfB
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.