2024-02-08 6:10 AM
Hi all,
I have a project on a STM32F7 target and I work on STM32CubeIDE.
How can I generate the binaries from the code ? And how can I flash the binaries in the STM32F7 (in NUCLEO-STM32F7ZG board) ?
I don't want to use the "flash" button of the app, as if I was a client with only binaries of the code.
Thank you for your help.
Best regards
Solved! Go to Solution.
2024-02-08 12:34 PM
@Remi99 The STM32CubeIDE also generates BIN files directly if you tick Convert to binary file in:
Project > Properties > C/C++ Build > Settings > MCU Post build outputs
NUCLEO boards like yours do not necessarily need a dedicated programming software because the embedded ST-LINK/V2-1 is visible as a mass storage device when connected to the PC via USB. The BIN can then be copied there using the normal copy command of the operating system, the ST-LINK/V2-1 then takes over the programming of the target.
2024-02-08 6:21 AM
Use STM32CubeProgrammer to flash a binary file (ELF, HEX, or BIN). When you compile code in STM32CubeIDE, this file is produces and put into the Debug/ or Release/ directory within the project.
2024-02-08 9:52 AM
OBJCOPY should be able to generate .BIN files from .ELF, FROMELF too
Host of other applications capable of converting HEX to BIN
Programming NUCLEO board, just use STM32 Cube Programmer. ST-LINK Utilities should also be fine with ST-LINK/V2 and F7 devices.
2024-02-08 12:34 PM
@Remi99 The STM32CubeIDE also generates BIN files directly if you tick Convert to binary file in:
Project > Properties > C/C++ Build > Settings > MCU Post build outputs
NUCLEO boards like yours do not necessarily need a dedicated programming software because the embedded ST-LINK/V2-1 is visible as a mass storage device when connected to the PC via USB. The BIN can then be copied there using the normal copy command of the operating system, the ST-LINK/V2-1 then takes over the programming of the target.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.