2023-09-06 9:24 AM
Hi,
I can't seem to get rid of this error. I am using the stm32h7b3i-dk board connected from mini-usb to usb on pc. File is present in the target folder. Anyone have any pointers?
Error in final launch sequence:
Failed to execute MI command:
load /Users/STM32CubeIDE/workspace_1.13.1/LedToggling/STM32CubeIDE/BootROM_ExternalSDRAM_InternalSRAM.Debug/LedToggling.elf
Error message from debugger back end:
Load failed
Failed to execute MI command:
load /Users/STM32CubeIDE/workspace_1.13.1/LedToggling/STM32CubeIDE/BootROM_ExternalSDRAM_InternalSRAM.Debug/LedToggling.elf
Error message from debugger back end:
Load failed
Failed to execute MI command:
load /Users/STM32CubeIDE/workspace_1.13.1/LedToggling/STM32CubeIDE/BootROM_ExternalSDRAM_InternalSRAM.Debug/LedToggling.elf
Error message from debugger back end:
Load failed
Load failed
2023-09-07 8:42 AM - edited 2023-09-26 6:51 AM
Hello @basssiozzz and welcome to the community,
At first, try to check the proxy settings following these steps:
- Under Window --> Preferences--> Network Connections, activate Native provider
- Under Window --> Preferences--> Firmware Updater, click on Check Connection
don't forget Apply and Close, if the connection works.
Could you, also, try to:
- Power off the target board
- Disconnect the ST-LINK JTAG USB cable
- Re-connect it t the ST-LINK JTAG USB cable
- Power on the target board
- Check the debug configuration settings, such as the SWD/JTAG interface
- Start the GDB server with different port number
I hope this will help!
Thanks,
Rim
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.