2022-08-15 1:17 PM
I'm using an STM32L4 with STM32CubeIDE, bare metal, and using C++ along with Cube's C libraries. The compiler is the GCC/G++ supplied with STM32CubeIDE.
I have some dynamic memory usage in STL containers etc. I'm aware of the recommendation not to use dynamic memory on bare-metal embedded systems, but it is generally used only during initialization, minimizing the complications.
I would like to know how much of the heap I'm using, and found no way to do that. I saw discussions of __heapstats but it doesn't seem to be defined in this toolchain (?).
It doesn't have to be a programmatic way, if there is some internal data structure of newlib or whatever that I can watch while debugging that will suffice.
p.s.
I know the term "free heap space" is not very well defined, because of block sizes and fragmentation, but I suspect that in my case it's going to be one big free block.
any ideas?
Solved! Go to Solution.
2022-08-16 6:20 AM
The default GCC toolchain comes with newlib as std. C library. I think the contained heap allocator supports mallinfo() to retrieve some heap status information.
2022-08-17 5:34 AM
Hello @tinkerer42
The most generic way to detect stack/heap collisions during run-time would be to by inserting a "known pattern" inside the RAM-memory.
If this memory is completely overwritten then you will know that the heap and stack has collided...
I think there should be some previous ticket where we advised how customer how he can re-write the Reset_Handler to fill the unused RAM with a known pattern.
Have a look at this extension to startup code:
LoopFillZerobss:
ldr r3, = _ebss
cmp r2, r3
bcc FillZerobss
/* ============================ */
/* Fill space between Heap and stack with magic pattern */
ldr r2, =_ebss
mov r4, sp
movs r3, #0xa5a5a5a5 /* The magic pattern */
b LoopFillPattern
FillPattern:
str r3, [r2]
adds r2, r2, #4
LoopFillPattern:
cmp r2, r4
bcc FillPattern
/* Call static constructors */
bl __libc_init_array
Kind regards,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-08-17 6:15 AM
that's probably the most robust solution, I'll try that.
Thanks!
2022-08-17 8:47 AM
You specifically asked for the variable names and structures your build process was using. Perhaps that..
2022-08-17 8:48 AM
The original question, in its entirety, was originally Determine heap free space on STM32
2022-08-17 8:57 AM
I don't recall stack collision, or stack size, being the question. This would be a good way of determining the low water mark of the stack, and high water mark on the heap within that same space. Not very enlightening on the current state of heap or stack, or determine used/unused sections of the heap. The heaps here are pretty simplistic linked lists.
What if the stack and heap are in entirely different memory regions? What if _sbrk() worked properly? Having it assume it's in the same memory region, and that the current base of the stack is a safe bounding condition, really not inspiring confidence at this end.
2022-08-17 12:00 PM
oh, ok - I just hoped to know in advance what I'm looking for (from someone with experience with the specific compiler)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.