2022-08-15 1:17 PM
I'm using an STM32L4 with STM32CubeIDE, bare metal, and using C++ along with Cube's C libraries. The compiler is the GCC/G++ supplied with STM32CubeIDE.
I have some dynamic memory usage in STL containers etc. I'm aware of the recommendation not to use dynamic memory on bare-metal embedded systems, but it is generally used only during initialization, minimizing the complications.
I would like to know how much of the heap I'm using, and found no way to do that. I saw discussions of __heapstats but it doesn't seem to be defined in this toolchain (?).
It doesn't have to be a programmatic way, if there is some internal data structure of newlib or whatever that I can watch while debugging that will suffice.
p.s.
I know the term "free heap space" is not very well defined, because of block sizes and fragmentation, but I suspect that in my case it's going to be one big free block.
any ideas?
Solved! Go to Solution.
2022-08-17 5:34 AM
Hello @tinkerer42
The most generic way to detect stack/heap collisions during run-time would be to by inserting a "known pattern" inside the RAM-memory.
If this memory is completely overwritten then you will know that the heap and stack has collided...
I think there should be some previous ticket where we advised how customer how he can re-write the Reset_Handler to fill the unused RAM with a known pattern.
Have a look at this extension to startup code:
LoopFillZerobss:
ldr r3, = _ebss
cmp r2, r3
bcc FillZerobss
/* ============================ */
/* Fill space between Heap and stack with magic pattern */
ldr r2, =_ebss
mov r4, sp
movs r3, #0xa5a5a5a5 /* The magic pattern */
b LoopFillPattern
FillPattern:
str r3, [r2]
adds r2, r2, #4
LoopFillPattern:
cmp r2, r4
bcc FillPattern
/* Call static constructors */
bl __libc_init_array
Kind regards,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-08-15 1:21 PM
Walk the linked list the allocator uses..
2022-08-15 1:26 PM
thanks, not pretty but I'll do it if there's no built-in lib to do it for me. I'd like to ask then -
the compiler is the GCC / G++ supplied with STM32CubeIDE, by the way.
2022-08-15 1:36 PM
The question looks more expansive now.
I'm using Keil.
__microlib_freelist_initialised
__microlib_freelist
The structure is ahead of the pointer returned by malloc()
2022-08-15 2:04 PM
Thanks, can anyone provide a similar answer for STM32CubeIDE's toolchain?
2022-08-15 2:42 PM
I'd have thought you could objcopy or fromelf the symbol and disassembly/listing of the code.
https://community.st.com/s/question/0D53W00000e0zTdSAI/malloc1
https://code.woboq.org/userspace/glibc/malloc/malloc.c.html
2022-08-15 3:49 PM
Why not union your variables with main global ones if they are exclusied in sequence, saving mallocs logic? (Manual clearing.maybe needed)
2022-08-15 5:03 PM
Dynamic allocation has its place, especially allocating buffers and objects at start-up, and where the usage might be configurable, or transitory
Now obviously using it like you would on a desktop, with no regard to leaks, or balance, that's a problem. Using it continuously is also not particularly advisable.
Then again using globals in an excessive and sloppy manner is also something to be avoided.
2022-08-15 7:04 PM
the short answer is that it leads me to cleaner code: using STL containers and other C++ features. The longer answer is that it has advantages and disadvantages, it is a common heated arguing point in the embedded community. I would really prefer NOT to open this discussion here, as it would completely distract from my original question.
So: does anyone know how to check heap free space when using the STM32CubeIDE toolchain?
2022-08-15 7:06 PM
What would I do with looking at the ELF etc? as they are the results of compilation and therefore know nothing about the runtime state of the heap?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.