2025-07-29 6:37 PM
Is it possible to edit the objcopy command emitted by the Stm32CubeIDEIDE? I need to make some adjustments to keep some RAM addresses from showing up in the hex file. Advice on the internet seems to thing this is easily adjustable in the IDE. However, I do not see any place where this can be modified.
Thanks,
Carl
2025-07-29 10:18 PM
> Advice on the internet
The internet is full of everything.
At least you can add a custom post-build command which could mimic the original objcopy with your adjustments and generate an additional output file.
> keep some RAM addresses from showing up in the hex file
Maybe you can adapt the .ld file here?
hth
KnarfB
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.