2023-08-12
3:53 AM
- last edited on
2024-05-22
9:01 AM
by
Lina_DABASINSKA
I don't care if the title of this post breaks some sort of forum usage rule, I just need to make it absolutely plain that I am sick and tired of every last company on Earth insisting I have an account with them and use it whenever I so much as breathe, drink a glass of water or, Chtuluh forbid ! update a HAL library for a microcontroller.
I believe there are more than enough bugs in CubeIDE, let alone actual necessary features that are missing, to keep your developers occupied forever. You did not need to waste everyone's time forcing people to login to ST. This feature brings nothing, helps no one but yourselves, and was asked by absolutely nobody, ever. So please, may I suggest you rethink this stupid, bordering on evil new addition to CubeIDE, and remove it with the next version ?
FYI, some of us work in companies where our computers are not, must not and cannot be, connected to the internet. It's already tough enough installing some of your HAL libraries (the patches) while being offline, we do not need the additional hassle of a login system that does nothing useful anyway.
A tool has to be convenient. If my screwdriver required an internet connection so as to snitch on how many turns I do in each direction depending on my GPS location, I'd start considering switching to fingernails or rocks.
You are welcome to try and make a case as to why you need me to log in to download updates to stuff you provide free of charge. I do need a good laugh.
Oh and I haven't checked on my last CubeIDE ticket... did you finally fix the bug where CubeIDE is confused when launching firmware on a target with Flash banks swapped ? Because that would sure be of actual use to the legions of programmers doing FOTA.
Solved! Go to Solution.
2023-09-10 12:30 PM
Hello, I have 10 nucleo-L476RG for students in my school. In my studio, there is a system for restoring computers from an image and I cannot allow students to log in to their st.com account. Is it possible to install drivers and libraries for the board without logging in to the st.com account? Alternatively, is it possible to create an account and log in to the account from 10 computers at the same time?
2023-09-10 2:21 PM - edited 2023-09-10 2:24 PM
@rutrap Since the logon is needed only for updating/installing stuff, you make a "master" setup using your own account, test it, remove your login info (*) and finally provision this image to all student stations. Students in this scenario are not supposed to modify their setup.
How to remove the login info? Search for it in the registry (Windows only) or user files.
2023-09-12 12:15 PM
Thank you for your answer, I will try it tomorrow and let you know. However, I think it should be possible to install library updates without logging in. In my case, I will have to update the libraries in the image myself from time to time.
2023-09-12 1:32 PM - edited 2023-09-12 1:34 PM
Yes it is possible to unpack and install the Cube firmware libraries manually without logging in. At least it worked before the latest CubeMX/IDE update. But you still have to log in to download them. You can also get most of the released versions from github, without login.
2023-09-12 2:06 PM
Agree, the forced login is simply uncalled for. There is no clear benefit to the users and no potential benefit to any increase in ease of use or productivity. Please provide a clear advantage to its use or remove it.
2023-09-13 2:01 PM
The advantage is that an educated manager Walter can tick a box in his PowerPoint presentation and explain to the bosses how they improved the enjoyable cohesive experience.
@STOne-32 , @mattias norlander , @KDJEM.1 , @Khouloud ZEMMELI , pass this post to the ones, who did this (especially the Walter), so that they can see themselves from aside...
2023-09-16 1:27 PM
Dear @Piranha , all,
As stated in previous post, we are considering your valuable feedback in order to provide best customer experience : Debug and Software tools ecosystems are now key factor for considering an MCU product in next project design at same level as its performance and features. As you can see here from last Embedded Survey - May 2023 with a panel over 600 experienced embedded engineering staff .
STM32CubeIDE is key element for STM32 MCU/MPU ecosystem and we can not ignore your valuable feedbacks. Our Marketing and Technical teams will take it into account in the future roadmap for our customers best experience.
by the way, very nice nickname “Piranha”- it was the internal project code name for the very first and famous MCU STM32F103XB :) I was among the team working on it :)
Cheers,
STOne-32
2023-09-19 7:14 PM
There are a number of things to consider:
2023-09-20 11:10 PM
Wow, could not have said it better.
2023-09-21 1:17 PM - edited 2023-09-21 1:18 PM
But look again at #2: he wants the tools and tutorials to be free, but in real world there is no free. Someone has to pay for it. We end users usually have to pay with our time and effort. Or we can pay someone else for their time and effort.
Good educators are rare, this is a special talent and it is scarce. /* My hope is with the AI: imagine a consultant that always has time for you, never bored, ingests tons of code, manuals, errata in a second. But this sounds too good for us to get? */
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.