2024-10-01 4:51 AM - edited 2024-10-01 4:52 AM
I am using CubeIDE version 1.16.1 to program and flash a STM32F433 MCU.
I am using a SEGGER J-Link flasher.
When I try to run the application I get the following error:
I have tried to manually set the workspace toolchain to local in the toolchain manager.
When I open the toolchain manager, I get an error that it has failed to fetch the toolchain list, in addition to four repositories that it cannot read:
Ignoring the message and setting the local toolchain as it follows
I get the same error when running the code on the MCU:
What should I try to do to fix the error?
2024-10-11 6:27 AM
Hello @Ghofrane GSOURI
here is my log where i login in as normal user and try to run debugging:
2024-10-11 15:16:03,461 [INFO] Activator:177 - !SESSION log4j initialized
2024-10-11 15:16:22,357 [INFO] LogOutputStream:77 - [STDOUT_REDIRECT]
2024-10-11 15:16:24,907 [ERROR] ConfigurationRetriever:142 - IOException on connection: Connect timed out
2024-10-11 15:16:25,049 [INFO] ApplicationProperties:184 - Using Application install path: C:\ST\STM32CubeIDE_1.16.1\STM32CubeIDE\plugins\com.st.stm32cube.common.mx_6.12.1.202409122256
2024-10-11 15:16:25,064 [INFO] DbMcusXml:78 - Set database path to: C:\ST\STM32CubeIDE_1.16.1\STM32CubeIDE\plugins\com.st.stm32cube.common.mx_6.12.1.202409122256\\db\/mcu/
2024-10-11 15:16:25,065 [INFO] ApiDb:274 - Set plugin database path to: C:\ST\STM32CubeIDE_1.16.1\STM32CubeIDE\plugins\com.st.stm32cube.common.mx_6.12.1.202409122256\\db\/plugins/boardmanager/
2024-10-11 15:16:25,065 [WARN] ApiDb:259 - Overriding images path with different value: => C:\ST\STM32CubeIDE_1.16.1\STM32CubeIDE\plugins\com.st.stm32cube.common.mx_6.12.1.202409122256\\db\/plugins/mcufinder/images/
2024-10-11 15:16:25,072 [INFO] ApiDb:250 - Set database path to: C:\Users\USER\.stmcufinder\plugins\mcufinder//mcu/
2024-10-11 15:16:25,073 [INFO] DbMcusAds:125 - Set database path to: C:\Users\USER\.stmcufinder\plugins\mcufinder//mcu/
2024-10-11 15:16:25,076 [INFO] CrossReferenceDbSqlite:203 - Set database path to: C:\Users\USER\.stmcufinder\plugins\mcufinder//mcu/cs/
2024-10-11 15:16:25,160 [INFO] RulesReader:64 - Compatibility file has been processed (297 Rules)
2024-10-11 15:16:25,233 [INFO] DbMcusXml:78 - Set database path to: C:\ST\STM32CubeIDE_1.16.1\STM32CubeIDE\plugins\com.st.stm32cube.common.mx_6.12.1.202409122256\\db\/mcu/
2024-10-11 15:16:25,233 [INFO] ApiDb:274 - Set plugin database path to: C:\ST\STM32CubeIDE_1.16.1\STM32CubeIDE\plugins\com.st.stm32cube.common.mx_6.12.1.202409122256\\db\/plugins/boardmanager/
2024-10-11 15:16:25,233 [INFO] ApiDb:261 - Set plugin images path to: C:\ST\STM32CubeIDE_1.16.1\STM32CubeIDE\plugins\com.st.stm32cube.common.mx_6.12.1.202409122256\\db\/plugins/mcufinder/images/
2024-10-11 15:16:25,233 [WARN] DbFile:41 - Overriding database path with different value: C:\Users\USER\.stmcufinder\plugins\mcufinder/ => C:\Users\USER\.stmcufinder\plugins\mcufinder
2024-10-11 15:16:25,233 [INFO] ApiDb:250 - Set database path to: C:\Users\USER\.stmcufinder\plugins\mcufinder//mcu/
2024-10-11 15:16:25,233 [WARN] DbFile:41 - Overriding database path with different value: C:\Users\USER\.stmcufinder\plugins\mcufinder/ => C:\Users\USER\.stmcufinder\plugins\mcufinder
2024-10-11 15:16:25,233 [INFO] DbMcusAds:125 - Set database path to: C:\Users\USER\.stmcufinder\plugins\mcufinder//mcu/
2024-10-11 15:16:25,233 [WARN] DbFile:41 - Overriding database path with different value: C:\Users\USER\.stmcufinder\plugins\mcufinder/ => C:\Users\USER\.stmcufinder\plugins\mcufinder
2024-10-11 15:16:25,233 [WARN] DbFile:41 - Overriding database path with different value: C:\Users\USER\.stmcufinder\plugins\mcufinder/ => C:\Users\USER\.stmcufinder\plugins\mcufinder
2024-10-11 15:16:25,233 [INFO] CrossReferenceDbSqlite:203 - Set database path to: C:\Users\USER\.stmcufinder\plugins\mcufinder//mcu/cs/
2024-10-11 15:16:25,299 [INFO] MainPanel:268 - HeapMemory: 367001600
2024-10-11 15:16:25,383 [INFO] DbMcusXml:78 - Set database path to: C:\ST\STM32CubeIDE_1.16.1\STM32CubeIDE\plugins\com.st.stm32cube.common.mx_6.12.1.202409122256\\db\/mcu/
2024-10-11 15:16:25,383 [INFO] ApiDb:274 - Set plugin database path to: C:\ST\STM32CubeIDE_1.16.1\STM32CubeIDE\plugins\com.st.stm32cube.common.mx_6.12.1.202409122256\\db\/plugins/boardmanager/
2024-10-11 15:16:25,384 [INFO] ApiDb:261 - Set plugin images path to: C:\ST\STM32CubeIDE_1.16.1\STM32CubeIDE\plugins\com.st.stm32cube.common.mx_6.12.1.202409122256\\db\/plugins/mcufinder/images/
2024-10-11 15:16:25,384 [WARN] DbFile:41 - Overriding database path with different value: C:\Users\USER\.stmcufinder\plugins\mcufinder/ => C:\Users\USER\.stmcufinder\plugins\mcufinder
2024-10-11 15:16:25,384 [INFO] ApiDb:250 - Set database path to: C:\Users\USER\.stmcufinder\plugins\mcufinder//mcu/
2024-10-11 15:16:25,384 [WARN] DbFile:41 - Overriding database path with different value: C:\Users\USER\.stmcufinder\plugins\mcufinder/ => C:\Users\USER\.stmcufinder\plugins\mcufinder
2024-10-11 15:16:25,384 [INFO] DbMcusAds:125 - Set database path to: C:\Users\USER\.stmcufinder\plugins\mcufinder//mcu/
2024-10-11 15:16:25,384 [WARN] DbFile:41 - Overriding database path with different value: C:\Users\USER\.stmcufinder\plugins\mcufinder/ => C:\Users\USER\.stmcufinder\plugins\mcufinder
2024-10-11 15:16:25,384 [WARN] DbFile:41 - Overriding database path with different value: C:\Users\USER\.stmcufinder\plugins\mcufinder/ => C:\Users\USER\.stmcufinder\plugins\mcufinder
2024-10-11 15:16:25,384 [INFO] CrossReferenceDbSqlite:203 - Set database path to: C:\Users\USER\.stmcufinder\plugins\mcufinder//mcu/cs/
2024-10-11 15:16:25,398 [INFO] ApplicationProperties:184 - Using Application install path: C:\ST\STM32CubeIDE_1.16.1\STM32CubeIDE\plugins\com.st.stm32cube.common.mx_6.12.1.202409122256
2024-10-11 15:16:25,399 [INFO] PluginManage:196 - Search for loadable plugins [exclusion list=, ]
2024-10-11 15:16:25,400 [INFO] PluginManage:310 - Check plugin analytics
2024-10-11 15:16:25,507 [INFO] AnalyticsPlugin:253 - Accepted Software Licenses:
2024-10-11 15:16:25,507 [INFO] AnalyticsPlugin:255 - Accepted CMSIS Pack Licenses:
2024-10-11 15:16:25,507 [INFO] AnalyticsPlugin:257 - Accepted Firmware Licenses: FW.F4.1.27.0,FW.H7.1.11.0,FW.F4.1.28.0
2024-10-11 15:16:25,510 [INFO] PluginManage:359 - Loaded plugin analytics (category:tool,tabindex:-1)
2024-10-11 15:16:25,510 [INFO] PluginManage:310 - Check plugin cadmodel
2024-10-11 15:16:25,527 [INFO] CADModel:105 - Init CAD model plugin
2024-10-11 15:16:25,527 [INFO] PluginManage:359 - Loaded plugin cadmodel (category:power,tabindex:5)
2024-10-11 15:16:25,527 [INFO] PluginManage:310 - Check plugin clock
...
...
2024-10-11 15:16:26,884 [INFO] PluginManager:220 - loadIPPluginJar : add stm32_wpan
2024-10-11 15:16:26,892 [INFO] IPUIPlugin:80 - create IPUIPlugin
2024-10-11 15:16:26,892 [INFO] PluginManager:220 - loadIPPluginJar : add tim
2024-10-11 15:16:26,902 [INFO] IPUIPlugin:80 - create IPUIPlugin
2024-10-11 15:16:26,902 [INFO] PluginManager:220 - loadIPPluginJar : add touchsensing
2024-10-11 15:16:26,908 [ERROR] ConfigurationRetriever:142 - IOException on connection: Connect timed out
2024-10-11 15:16:26,910 [INFO] IPUIPlugin:80 - create IPUIPlugin
2024-10-11 15:16:26,910 [INFO] PluginManager:220 - loadIPPluginJar : add tracer_emb
2024-10-11 15:16:26,919 [INFO] IPUIPlugin:80 - create IPUIPlugin
2024-10-11 15:16:26,919 [INFO] PluginManager:220 - loadIPPluginJar : add ts
2024-10-11 15:16:26,927 [INFO] IPUIPlugin:80 - create IPUIPlugin
2024-10-11 15:16:26,927 [INFO] PluginManager:220 - loadIPPluginJar : add tsc
2024-10-11 15:16:26,935 [INFO] IPUIPlugin:80 - create IPUIPlugin
2024-10-11 15:16:26,935 [INFO] PluginManager:220 - loadIPPluginJar : add ucpd
2024-10-11 15:16:26,943 [INFO] IPUIPlugin:80 - create IPUIPlugin
2024-10-11 15:16:26,944 [INFO] PluginManager:220 - loadIPPluginJar : add usart
2024-10-11 15:16:26,952 [INFO] IPUIPlugin:80 - create IPUIPlugin
2024-10-11 15:16:26,952 [INFO] PluginManager:220 - loadIPPluginJar : add usbx
2024-10-11 15:16:27,061 [INFO] CADModel:165 - CPN selected for project level
2024-10-11 15:16:27,061 [INFO] CADModel:114 - Register for checkConnection events
2024-10-11 15:16:27,061 [FATAL] Updater:334 - Updater called before beeing initialized
2024-10-11 15:16:27,061 [ERROR] CADModel:125 - Updater not yet initialized, retry later
2024-10-11 15:16:27,152 [INFO] CADModel:165 - CPN selected for project level
2024-10-11 15:16:27,152 [INFO] CADModel:114 - Register for checkConnection events
2024-10-11 15:16:27,152 [FATAL] Updater:334 - Updater called before beeing initialized
2024-10-11 15:16:27,152 [ERROR] CADModel:125 - Updater not yet initialized, retry later
2024-10-11 15:16:27,155 [FATAL] Updater:334 - Updater called before beeing initialized
2024-10-11 15:16:27,231 [FATAL] Updater:334 - Updater called before beeing initialized
2024-10-11 15:16:27,236 [INFO] DbMcusAds:53 - JSON generation date=Fri Sep 20 15:04:23 CEST 2024 (1726837463113)
2024-10-11 15:16:27,236 [FATAL] Updater:334 - Updater called before beeing initialized
2024-10-11 15:16:27,300 [WARN] DetailPanel:346 - Failed to get advertising image, set to default
2024-10-11 15:16:27,361 [FATAL] Updater:334 - Updater called before beeing initialized
2024-10-11 15:16:27,362 [FATAL] Updater:334 - Updater called before beeing initialized
2024-10-11 15:16:27,362 [FATAL] Updater:334 - Updater called before beeing initialized
2024-10-11 15:16:27,362 [WARN] DetailPanel:346 - Failed to get advertising image, set to default
2024-10-11 15:16:27,362 [FATAL] Updater:334 - Updater called before beeing initialized
2024-10-11 15:16:27,398 [ERROR] Updater:1164 - MainUpdater not yet initialized. External WinMGr cannot be set.
2024-10-11 15:16:27,402 [INFO] Updater:1100 - Updater Version found : 6.12.1
2024-10-11 15:16:27,416 [INFO] ApplicationProperties:184 - Using Application install path: C:\ST\STM32CubeIDE_1.16.1\STM32CubeIDE\plugins\com.st.stm32cube.common.mx_6.12.1.202409122256
2024-10-11 15:16:28,909 [ERROR] ConfigurationRetriever:142 - IOException on connection: Connect timed out
2024-10-11 15:16:29,081 [INFO] ThirdPartyUpdaterWithRetryManager:70 - Updater plugin not ready yet. [2/15]
2024-10-11 15:16:30,511 [ERROR] ConfigurationRetriever:142 - IOException on connection: Connect timed out
2024-10-11 15:16:31,593 [WARN] CheckConnectionManager:291 - Warning during Server Connection : timeout Connect to sw-center.st.com:443 [sw-center.st.com/23.53.40.64, sw-center.st.com/23.53.40.26] failed: Connect timed out
2024-10-11 15:16:32,084 [FATAL] Updater:334 - Updater called before beeing initialized
2024-10-11 15:16:32,084 [ERROR] IntegrityCheckThread:130 - Cannot retrieve database content from updater: error 21
2024-10-11 15:16:32,084 [INFO] ThirdParty:978 - Integrity check success = false
2024-10-11 15:16:32,084 [INFO] IntegrityCheckThread:100 - exiting critical section [integrity check]
2024-10-11 15:16:32,084 [INFO] IntegrityCheckThread:103 - End integrity checks thread
2024-10-11 15:16:35,514 [ERROR] ConfigurationRetriever:142 - IOException on connection: Connect timed out
2024-10-11 15:16:35,606 [WARN] CheckConnectionManager:291 - Warning during Server Connection : timeout Connect to sw-center.st.com:443 [sw-center.st.com/23.53.40.64, sw-center.st.com/23.53.40.26] failed: Connect timed out
2024-10-11 15:16:35,610 [INFO] MainUpdater:2873 - connection check result : 22
2024-10-11 15:16:35,611 [INFO] MainUpdater:290 - Updater Check For Update Now.
2024-10-11 15:16:35,611 [INFO] MicroXplorer:498 - Change Database Version : DB.6.0.121
2024-10-11 15:16:35,617 [INFO] McuFinderGlobals:63 - Set McuFinder mode to 2 (CubeIDE integrated)
2024-10-11 15:16:35,618 [INFO] UserAuth:417 - Internet connection configuration mode: 2
2024-10-11 15:16:35,625 [INFO] UserAuth:417 - Internet connection configuration mode: 2
2024-10-11 15:16:35,766 [INFO] CheckServerUpdateThread:120 - End of CheckServer Thread
2024-10-11 15:16:40,517 [ERROR] ConfigurationRetriever:142 - IOException on connection: Connect timed out
2024-10-11 15:16:48,697 [ERROR] ConfigurationRetriever:142 - IOException on connection: Connect timed out
2024-10-11 15:16:50,698 [ERROR] ConfigurationRetriever:142 - IOException on connection: Connect timed out
2024-10-11 15:16:52,699 [ERROR] ConfigurationRetriever:142 - IOException on connection: Connect timed out
2024-10-11 15:17:13,545 [WARN] CheckConnectionManager:291 - Warning during Server Connection : timeout Connect to sw-center.st.com:443 [sw-center.st.com/23.48.23.46, sw-center.st.com/23.48.23.61] failed: Connect timed out
2024-10-11 15:17:15,550 [WARN] CheckConnectionManager:291 - Warning during Server Connection : timeout Connect to sw-center.st.com:443 [sw-center.st.com/23.48.23.46, sw-center.st.com/23.48.23.61] failed: Connect timed out
2024-10-11 15:17:15,551 [INFO] MainUpdater:2873 - connection check result : 22
2024-10-11 15:17:17,560 [WARN] CheckConnectionManager:291 - Warning during Server Connection : timeout Connect to sw-center.st.com:443 [sw-center.st.com/23.48.23.46, sw-center.st.com/23.48.23.61] failed: Connect timed out
2024-10-11 15:17:19,564 [WARN] CheckConnectionManager:291 - Warning during Server Connection : timeout Connect to sw-center.st.com:443 [sw-center.st.com/23.48.23.46, sw-center.st.com/23.48.23.61] failed: Connect timed out
2024-10-11 15:17:19,566 [INFO] MainUpdater:2873 - connection check result : 22
2024-10-11 15:17:32,433 [WARN] CheckConnectionManager:291 - Warning during Server Connection : timeout Connect to sw-center.st.com:443 [sw-center.st.com/23.53.40.26, sw-center.st.com/23.53.40.64] failed: Connect timed out
2024-10-11 15:17:34,438 [WARN] CheckConnectionManager:291 - Warning during Server Connection : timeout Connect to sw-center.st.com:443 [sw-center.st.com/23.53.40.26, sw-center.st.com/23.53.40.64] failed: Connect timed out
2024-10-11 15:17:34,439 [INFO] MainUpdater:2873 - connection check result : 22
2024-10-11 15:17:36,446 [WARN] CheckConnectionManager:291 - Warning during Server Connection : timeout Connect to sw-center.st.com:443 [sw-center.st.com/23.53.40.26, sw-center.st.com/23.53.40.64] failed: Connect timed out
2024-10-11 15:17:38,449 [WARN] CheckConnectionManager:291 - Warning during Server Connection : timeout Connect to sw-center.st.com:443 [sw-center.st.com/23.53.40.26, sw-center.st.com/23.53.40.64] failed: Connect timed out
2024-10-11 15:17:38,450 [INFO] MainUpdater:2873 - connection check result : 22
2024-10-11 15:17:40,471 [WARN] CheckConnectionManager:291 - Warning during Server Connection : timeout Connect to sw-center.st.com:443 [sw-center.st.com/23.53.40.26, sw-center.st.com/23.53.40.64] failed: Connect timed out
2024-10-11 15:17:42,478 [WARN] CheckConnectionManager:291 - Warning during Server Connection : timeout Connect to sw-center.st.com:443 [sw-center.st.com/23.53.40.26, sw-center.st.com/23.53.40.64] failed: Connect timed out
2024-10-11 15:17:42,480 [INFO] MainUpdater:2873 - connection check result : 22
2024-10-11 15:17:44,484 [WARN] CheckConnectionManager:291 - Warning during Server Connection : timeout Connect to sw-center.st.com:443 [sw-center.st.com/23.53.40.26, sw-center.st.com/23.53.40.64] failed: Connect timed out
2024-10-11 15:17:46,496 [WARN] CheckConnectionManager:291 - Warning during Server Connection : timeout Connect to sw-center.st.com:443 [sw-center.st.com/23.53.40.26, sw-center.st.com/23.53.40.64] failed: Connect timed out
2024-10-11 15:17:46,497 [INFO] MainUpdater:2873 - connection check result : 22
2024-10-11 15:18:22,292 [WARN] CheckConnectionManager:291 - Warning during Server Connection : timeout Connect to sw-center.st.com:443 [sw-center.st.com/23.213.161.27, sw-center.st.com/23.213.161.22] failed: Connect timed out
2024-10-11 15:18:24,296 [WARN] CheckConnectionManager:291 - Warning during Server Connection : timeout Connect to sw-center.st.com:443 [sw-center.st.com/23.213.161.27, sw-center.st.com/23.213.161.22] failed: Connect timed out
2024-10-11 15:18:24,298 [INFO] MainUpdater:2873 - connection check result : 22
2024-10-11 15:18:26,303 [WARN] CheckConnectionManager:291 - Warning during Server Connection : timeout Connect to sw-center.st.com:443 [sw-center.st.com/23.213.161.27, sw-center.st.com/23.213.161.22] failed: Connect timed out
2024-10-11 15:18:28,306 [WARN] CheckConnectionManager:291 - Warning during Server Connection : timeout Connect to sw-center.st.com:443 [sw-center.st.com/23.213.161.27, sw-center.st.com/23.213.161.22] failed: Connect timed out
2024-10-11 15:18:28,308 [INFO] MainUpdater:2873 - connection check result : 22
2024-10-11 15:18:35,777 [WARN] CheckConnectionManager:291 - Warning during Server Connection : timeout Connect to sw-center.st.com:443 [sw-center.st.com/23.213.161.27, sw-center.st.com/23.213.161.22] failed: Connect timed out
2024-10-11 15:18:37,782 [WARN] CheckConnectionManager:291 - Warning during Server Connection : timeout Connect to sw-center.st.com:443 [sw-center.st.com/23.213.161.27, sw-center.st.com/23.213.161.22] failed: Connect timed out
2024-10-11 15:18:37,784 [INFO] MainUpdater:2873 - connection check result : 22
2024-10-11 15:18:39,788 [WARN] CheckConnectionManager:291 - Warning during Server Connection : timeout Connect to sw-center.st.com:443 [sw-center.st.com/23.213.161.27, sw-center.st.com/23.213.161.22] failed: Connect timed out
2024-10-11 15:18:41,791 [WARN] CheckConnectionManager:291 - Warning during Server Connection : timeout Connect to sw-center.st.com:443 [sw-center.st.com/23.213.161.27, sw-center.st.com/23.213.161.22] failed: Connect timed out
2024-10-11 15:18:41,793 [INFO] MainUpdater:2873 - connection check result : 22
2024-11-21 11:35 PM
Hi,
Could you understand anything from my log?
I also wanted to ask if you could give me all the URLs I need to allow the STM32 Cube IDE to run properly?
Thanks for your help.
2024-11-22 6:26 AM
I had the same problem. I had to reinstall the ide. My guess is another update coming soon.
2025-05-14 10:28 AM
I just had the error, too. Despite compiling working just fine, when going to debugging, with a previously working, and unchanged (according to git) debug configuration, the thing claims, "arm-none-eabi-gdb --version" to not work.
The only thing that helped was to close the IDE, delete the ".metadata" (might be hidden on your system depending on explorer settings, if on Windows) folder, restart the IDE, and the you have to re-import the project(s) in the workspace.
Via menu: File -> Import... -> General/Existing Projects into Workspace.
Select the proper root directory, and it will serch through the folder and list the projects it finds. Check the boxes of those you want to import.
Then, also with the File -> Import menu, this time, the "Run/Debug" folder -> "Launch Configurations", you'll have to import your debug configurations again.
I recommend keeping all those in a subfolder in your workspace or project folder.
Then, I also had to open the toolchain manager and "add local" the toolchain I was using, giving it the proper name handle (like "GCC13.3" or so) which your project is set up to use...
Therafter, building again and debugging worked.
I have no idea what put the IDE data that is in .metadata in this weird state... but this happens sometimes.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.