2021-05-25 8:35 AM
I've done plenty of bootloaders over the ywars for the STM32 using Crossworks. When I want to set the program to start from a differemt location I simply set a macro in the project properies to the address at which I want the program to reside, then recompile.
How do I do that with the Cube IDE please?
Thanks!
2021-05-25 8:49 AM
Would look at the Linker Script (and related linker dialogs), and fix SystemInit() code to set SCB->VTOR correctly, ideally with symbols the linker is already using/generating.
2021-05-25 9:00 AM
I'm not worried about the VTOR, that's a different thing and won't change between IDEs (I don't see why it would anyway). Am happy I know what to do there (famous last words).
I'd pretty much guessed I *might* have to deal with the linker rather than putting a macro statement into the project properties as with Crossworks. However, I'm not sure whether it's as simple as changing:
FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 1024K
to
FLASH (rx) : ORIGIN = 0x8008000, LENGTH = 992K
As far as Linker dialogues are concerned, if you're talking about Eclipse dialogues, I can see nothing that helps, hence asking.
2021-05-25 10:06 AM
Yes as simple ;)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.