2025-05-22 8:53 AM
I'm using STM32CubeIDE 1.18.1 and when i create a new STM32 CMake Project for a STM32U5, the generated ld file contain only half the memory.
For example here what is generated in STM32U575ZITXQ_FLASH.ld:
MEMORY
{
RAM (xrw) : ORIGIN = 0x20040000, LENGTH = 512K /* Memory is divided. Actual start is 0x20000000 and actual length is 768K */
SRAM4 (xrw) : ORIGIN = 0x28000000, LENGTH = 16K
FLASH (rx) : ORIGIN = 0x08100000, LENGTH = 1024K /* Memory is divided. Actual start is 0x08000000 and actual length is 2048K */
}This doesn't happens when creating a classic STM32 project.
Solved! Go to Solution.
2025-05-26 3:43 AM
Hello @nicolas ,
Let me thank you for bringing this issue to our attention.
An internal ticket is submitted to the Development Team (Ticket Number: 210768).
Thanks.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-05-22 9:11 AM
Hello @nicolas
First let me thank you for posting.
Your request is under investigation, and I will get back to you ASAP.
Thanks.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-05-23 1:55 AM
2025-05-23 2:09 AM
2025-05-26 3:43 AM
Hello @nicolas ,
Let me thank you for bringing this issue to our attention.
An internal ticket is submitted to the Development Team (Ticket Number: 210768).
Thanks.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.