2019-06-11 12:38 AM
Hi,
I am trying to port over the following startup commands from Atollic, but I realized when I place them in the initialization commands, the comment lines throw an error of Undefined Command. My script runs fine without the comments, but I thought it will be nice to be able to still include the comments.
Any idea how to add these comments in the new STM32CubeIDE?
# Reconfigure vector table offset register to match the application location
set *0xe000ed08 = 0xC000
# Get the application stack pointer (First entry in the application vector table)
set $sp = *(unsigned int*)0xC000
# Get the application entry point (Second entry in the application vector table)
set $pc = *(unsigned int*)0xC004
Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.