2020-01-18 9:08 AM
I'm new to STM32 development.
I use a STM32F407G-DISC1 kit.
When I create a new project in STM32CubeMX for this board, I get all my on-board components like LEDs, buttons etc. mapped in GPIO section. This is very handy, because these evaluation board often used for quick prototyping.
When I go through the same process in STM32CubeIDE, for some reason I/O is not mapped. I answer Yes to the "Initialize all peripherals with their default Mode" dialog, but the GPIO section remains empty.
Maybe I do something wrong here?
I can first generate a project in STM32CubeMX and then open it STM32CubeIDE, but I would definitely prefer if I could do both initial configuration and development withing one application.
I use the latest available veresion of STM32CubeIDE (v1.2.1).
Solved! Go to Solution.
2020-01-21 8:29 AM
I uninstalled all ST products, then installed SMT32CubeIDE and now everything works OK.
2020-01-20 1:38 PM
2020-01-21 8:29 AM
I uninstalled all ST products, then installed SMT32CubeIDE and now everything works OK.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.