2025-03-09 5:36 PM
Hello,
Is there a trick to get the Build Analyzer to produce data every time the code is compiled? It seems like the only way I can get it to update the window is if I change something in the linker script file and recompile again. Is there an easier way or a setting that needs to be set?
thanks
Matthew
Solved! Go to Solution.
2025-04-27 11:21 PM
I can confirm. It seems the trick is to:
2025-07-29 1:22 PM
This is an incredibly frustrating bug.
For me, none of the clicking and refreshing of the project works. The only alternative to rebooting the entire IDE I've found is to close the build analyzer before building, then building, then re-opening it from the Window menu and refreshing.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.