STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

execute nested functions in RAM on STM32F746

Hello, I'm trying to get running own external loader for CubeMX compiled with CubeIDE.I have followed this internet source to set-up envirement but without success. Because the CubeMX plugin doesn't work I tried to debug RAM-execution without CubeMX....

Wlad777 by Associate II
  • 1294 Views
  • 2 replies
  • 0 kudos

Make SWO character output non-blocking?

Correct me if I'm wrong, but it seems that ITM_SendChar() is blocking on the character transmission. Has anyone attempted to compensate for this or do people just put up/move to a UART?At this point all I can think of is to implement a FIFO queue and...

Grant Bt by Senior II
  • 1551 Views
  • 4 replies
  • 3 kudos

Tooltips background text is black and text not visible

Hi,In STM32CubeIDE code editor when I go over a variable or function the tool tip window that opens and shows the declaration of variable or implementation of the function  - the window has a black (very dark background ) and text is also black and n...

Screenshot 2025-05-11 085913.jpg
CSand by Associate III
  • 2036 Views
  • 4 replies
  • 0 kudos

STM32CubeIDE 1.18.1 Login Error

I have some problem, I Can't login STM32 IDE - 1.18.1 Version Manu : Help → STM32Cube updata → Connection to myST → Enter myST account information So, Open the Uset Authentication Dialog, but i can't see anything. i need help, please  

HongGu_0-1747876868232.png
HongGu by Associate
  • 568 Views
  • 1 replies
  • 0 kudos

are new, delete thread safe in FreeRTOS?

I have a dubt:I'm using c++, touchgfx and FreeRTOS: new and delete operators are thread safe ?   What they mean "Be warned that (at the time of writing) the current newlib design implements a system-wide malloc() that must be provided with locks" ? T...

MauFanGilaMedical_0-1747831774503.png MauFanGilaMedical_1-1747831843080.png

Resolved! Issue during stm32cube ide new update.

Hello team,For the development purpose, I want to update the stm32cube ide.I am updating ide from path "Help-> Check for updates"I am having following issue.An error occurred while collecting items to be installedsession context was:(profile=STM32Cub...

Rahuld by Associate III
  • 1820 Views
  • 4 replies
  • 2 kudos

VectorTable Fault

Hi I'm working on implementing a bootloader on a Nucleo H723ZG and attempted to relocate the application to a different flash address. During testing in the debugger, I found that the application only runs correctly when I explicitly specify the vect...

MFh1_0-1747833442005.png MFh1_3-1747833616484.png MFh1_1-1747833485422.png MFh1_2-1747833527004.png
MFäh.1 by Associate II
  • 572 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.