2019-07-22 8:48 AM
In dspin.h file
#define CHECK_REG(reg, result) if (dSPIN_RegsStruct-> ## reg != dSPIN_Get_Param(dSPIN_ ## reg)) result |= 1 << ((uint8_t) dSPIN_ ## reg)
Compiling error for dspin.c
uint32_t dSPIN_Registers_Check(dSPIN_RegsStruct_TypeDef* dSPIN_RegsStruct)
{
uint32_t result = 0;
CHECK_REG(ABS_POS, result);
make -j8 all
arm-none-eabi-gcc "../Src/dspin.c" -mcpu=cortex-m7 -std=gnu11 -g3 -DUSE_HAL_DRIVER -DSTM32F767xx -DDEBUG -c -I../Inc -I../Drivers/CMSIS/Include -I../Drivers/CMSIS/Device/ST/STM32F7xx/Include -I../Drivers/STM32F7xx_HAL_Driver/Inc -I../Drivers/STM32F7xx_HAL_Driver/Inc/Legacy -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -MMD -MP -MF"Src/dspin.d" -MT"Src/dspin.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Src/dspin.o"
arm-none-eabi-gcc "../Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_rcc.c" -mcpu=cortex-m7 -std=gnu11 -g3 -DUSE_HAL_DRIVER -DSTM32F767xx -DDEBUG -c -I../Inc -I../Drivers/CMSIS/Include -I../Drivers/CMSIS/Device/ST/STM32F7xx/Include -I../Drivers/STM32F7xx_HAL_Driver/Inc -I../Drivers/STM32F7xx_HAL_Driver/Inc/Legacy -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -MMD -MP -MF"Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_rcc.d" -MT"Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_rcc.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_rcc.o"
arm-none-eabi-gcc "../Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_rcc_ex.c" -mcpu=cortex-m7 -std=gnu11 -g3 -DUSE_HAL_DRIVER -DSTM32F767xx -DDEBUG -c -I../Inc -I../Drivers/CMSIS/Include -I../Drivers/CMSIS/Device/ST/STM32F7xx/Include -I../Drivers/STM32F7xx_HAL_Driver/Inc -I../Drivers/STM32F7xx_HAL_Driver/Inc/Legacy -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -MMD -MP -MF"Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_rcc_ex.d" -MT"Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_rcc_ex.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_rcc_ex.o"
arm-none-eabi-gcc "../Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_tim.c" -mcpu=cortex-m7 -std=gnu11 -g3 -DUSE_HAL_DRIVER -DSTM32F767xx -DDEBUG -c -I../Inc -I../Drivers/CMSIS/Include -I../Drivers/CMSIS/Device/ST/STM32F7xx/Include -I../Drivers/STM32F7xx_HAL_Driver/Inc -I../Drivers/STM32F7xx_HAL_Driver/Inc/Legacy -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -MMD -MP -MF"Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_tim.d" -MT"Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_tim.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_tim.o"
arm-none-eabi-gcc "../Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_tim_ex.c" -mcpu=cortex-m7 -std=gnu11 -g3 -DUSE_HAL_DRIVER -DSTM32F767xx -DDEBUG -c -I../Inc -I../Drivers/CMSIS/Include -I../Drivers/CMSIS/Device/ST/STM32F7xx/Include -I../Drivers/STM32F7xx_HAL_Driver/Inc -I../Drivers/STM32F7xx_HAL_Driver/Inc/Legacy -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -MMD -MP -MF"Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_tim_ex.d" -MT"Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_tim_ex.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_tim_ex.o"
In file included from ../Inc/dspin_config.h:27:0,
from ../Src/dspin.c:24:
../Src/dspin.c: In function 'dSPIN_Registers_Get':
../Inc/dspin.h:889:35: error: pasting "->" and "ABS_POS" does not give a valid preprocessing token
if (read_reg != dSPIN_RegsStruct-> ## reg_name) strcpy(diff,"x"); \
2019-07-22 8:56 AM
So grep project and see what ABS_POS is set to, and if you have missing or multiple instances of it.
2019-07-22 9:11 AM
Hi Clive,
Thanks for your reply. It looks like the compiler is not able to recognize the Macro token paste operator : ##. The compiler supposedly should be able to preprocess the macro CHECK_REF(ABS_POS, result) by replacing it with if (dSPIN_RegsStruct-> ABS_POS != dSPIN_Get_Param(dSPIN_ ABS_POS)) result |= 1 << ((uint8_t) dSPIN_ ABS_POS
Is there any option in the compiler I need to turn so that the compiler is able to support the Token Paste Operator : ##?
Thanks a lot.
2019-07-22 9:16 AM
Sounds more like it is working but one or more of the things it is trying to paste together is wrong.
Do any of the demo projects using dspin.c work/build properly?
Can you enable the compiler to output the pre-processor pass of the source so you can inspect/review that?
2019-07-22 9:24 AM
Do you know how? It seems I was not able to find such a compiler option setting. Thanks
2019-07-22 9:36 AM
" -E Stop after the preprocessing stage; do not run the compiler proper.
The output is in the form of preprocessed source code, which is sent to the standard output.
Input files that don't require preprocessing are ignored." https://manned.org/arm-none-eabi-gcc/34fd6095
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.