STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Error During creating new project in STCube v1.1.0

Goodevening,I'm new on this community and i I want to apologize in advance if I make some mistake. My problem is: when i create new STM32 project i get this error "Code generation could not be done because the necessary firmware package is missing. N...

There are a large number of existing STM32 sample projects set up to work with EWARM, MDK-ARM and SW4STM32. Even though use the migration guide for importing projects into STM32CubeIDE most of the time these projects do not import properly.

Are there any instructions on how to import an existing STM example project into STM32CubeIDE such that is can be built and deployed. At the moment its a very frustrating process that wastes lots of time and energy.

request: board examples using the CubeIDE project structure

When stumped, I've found that the examples in the various board zip files that STMCubeIDE downloads are very helpful. However none of them are structured in a way that I know how to load into the 'modern' STM32CubeIDE. is there any documentation aime...

mmalex by Associate II
  • 1280 Views
  • 1 replies
  • 0 kudos

Resolved! Why float X = 3300/2000 = 1?

I have a simple calculate#define VREF ((uint16_t) 3300)   float X = VREF / 2000;Why X result is 1? This happen with another calculate like xx00 / xx000Thanks

NNam.18 by Associate II
  • 2561 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.