2019-06-28 12:17 AM
As title.
When I open a .ioc MX configuration of a project with the newest version, the IDE hangs at "Initializing Device Configuration Tool".
2019-06-28 2:31 AM
I just did a test on my Windows and I can't reproduce this.
What operating system are you using?
And just to make sure:
You're creating a project in 1.0.0 and then you open it in 1.0.1 and when you try to edit in the .ioc file you get stuck at "Initializing Device Configuration Tool", right?
2019-06-28 2:33 AM
That is right.
I'm using Mac.
The project is configured with USART1 and USB CDC (STM32WB55).
2019-06-28 4:22 AM
I was able to reproduce it when I used a mac computer instead.
I'll make a ticket for it, thanks for the feedback!
2019-07-02 8:19 AM
I am having this same issue as well, and I am using Mac OSX 10.14.5
2019-07-02 8:32 AM
I was able to open the MX file if I edited the .ioc file to bump the version numbers. I made the following changes:
MxCube.Version=5.2.0 ==> MxCube.Version=5.2.1
MxDb.Version=DB.5.0.21 ==> MxDb.Version=DB.5.0.21
However, I do not know if this introduces any new errors, so proceed with caution.
2019-07-24 3:54 AM
I have just installed this on a Mac to see if I wanted to move from SW4STM32. I installed V1.0.1 and made a test project. Then I was told that there was a version 1.0.2 so I installed that. Now it hangs trying to open the ioc as the OP describes.
2019-10-28 1:15 AM
Same issue with 1.1. Is anyone fixing bugs?
2019-12-01 6:49 PM
Same problem with MX version 5.4.0. How do I find out what the correct MxDb.Version should be set to? Is there anything else I need to do to convert an '.ioc' file?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.