2019-11-29 4:17 PM
I'm using an STM32F030R8T6 chip on a breadboard. Everything works fine with Atollic TrueSTUDIO, but I decided to download STM32CubeIDE and create a basic empty project.
In the Device Configuration Tool, all I did was enable "Debug Serial Wire" so that I can debug using ST-Link. No user code in the main loop yet. After hitting the debug icon, this is output and I get a break point on HAL_Init()
STMicroelectronics ST-LINK GDB server. Version 5.3.2
Copyright (c) 2019, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
LogFile Name : C:\Users\me\STM32CubeIDE\workspace_1.1.0\test\Debug\st-link_gdbserver_log.txt
Logging Level : 31
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Enabled
SWD Debug : Enabled
Target connection mode: Attach
Hardware watchpoint supported by the target
COM frequency = 4000 kHz
ST-LINK Firmware version : V2J34S7
Device ID: 0x440
PC: 0xfffffffe
ST-LINK device status: HALT_MODE
ST-LINK detects target voltage = 3.28 V
ST-LINK device status: HALT_MODE
ST-LINK device initialization OK
Waiting for debugger connection...
Waiting for connection on port 61234...
Accepted connection on port 61234...
Debugger connected
Enter STM32_AppReset() function
NVIC_DFSR_REG = 0x0000000B
XPSR = 0xC1000003
------ Switching to STM32CubeProgrammer -----
-------------------------------------------------------------------
STM32CubeProgrammer v2.2.0
-------------------------------------------------------------------
Log output file: C:\Users\me\AppData\Local\Temp\STM32CubeProgrammer_a01452.log
ST-Link Server is running on port : 7184
ST-LINK SN : 48FF72066578555560290667
ST-LINK FW : V2J34S7
Voltage : 3.28V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x440
Device name : STM32F05x/F030x8
Flash size : 64 KBytes
Device type : MCU
Device CPU : Cortex-M0
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a01452.srec
File : ST-LINK_GDB_server_a01452.srec
Size : 3932 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 3]
Download in Progress:
�������������������������������������������������� 0%
�������������������������������������������������� 100%
File download complete
Time elapsed during download operation: 00:00:00.515
Verifying ...
Read progress:
�������������������������������������������������� 50%
�������������������������� 52%������������� 78%����������� 100%
Download verified successfully
------ Switching context -----
Target connection mode: Default
Hardware watchpoint supported by the target
COM frequency = 4000 kHz
ST-LINK Firmware version : V2J34S7
Device ID: 0x440
PC: 0x8000388
ST-LINK detects target voltage = 3.28 V
ST-LINK device status: HALT_MODE
ST-LINK device initialization OK
handle_vCont_c, continue thread
TraceCaptureStart and SWV event set to APP_FALSE (0)
NVIC_DFSR_REG = 0x0000000B
I then proceed to step into the SystemClock_Config() funtion until it eventually reaches the __HAL_RCC_PLL_ENABLE() funtion. After that, I lose the debugger and the console starts printing this:
handle_vCont_c, Failed step thread
ST-LINK device status: RUN_MODE
ST-LINK device status: Failed to get status, Target not responding, retrying...
Target is not responding, retrying...
..
..
ST-LINK device status: Failed to get status, Target not responding, retrying...
Target is not responding, retrying...
ST-LINK device status: TMO (Max Retries)
Debugger connection lost.
Shutting down...
Seems like the build is working, and the image is being loaded to the target, but something goes foul and causes the target to stop responding. Any suggestions would be greatly appreciated. I can provide any further information you need, or I can perform other steps if you offer them.
Thanks in advance,
Leo
Solved! Go to Solution.
2019-11-29 5:54 PM
2019-11-29 5:54 PM
Issue with Power or VDDA
Incorrect PLL values, or Flash wait states.
2019-11-30 3:10 PM
I didn't have VDDA/VSSA connected. After supplying VDDA/VSSA, everything is now working as expected. I suppose this wasn't a problem when I was using Atollic TrueSTUDIO it wasn't trying to enable PLL with initialization code.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.