STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32CubeIDE USB Host FS (1.5MBit/s) HID - Mini keyboard Touchpad Wireless is stopping responding when it enters standby or touchpad mode

Does anyone know how to make this keyboard work?With the MAX3421E chip in conjunction with the USH30 library this works but with STM32CubeIDE not working properly.https://www.amazon.com/Rii-Wireless-Keyboard-Touchpad%EF%BC%86QWERTY-Raspberry/dp/B00B9...

0690X00000AsNmkQAF.jpg
by Not applicable
  • 4193 Views
  • 11 replies
  • 0 kudos

"Breakpoint installation failed: unmatched quote" at CubeIDE

Hi, I’ve a problem trying to setup breakpoints. At any code line where I try to setup a breakpoint, it does not matter which, neither if it’s the main.c or a library, it just keeps telling me “Breakpoint installation failed: unmatched quote�? as you ...

Fèlix by Associate II
  • 2584 Views
  • 2 replies
  • 0 kudos

How to fix stm32Cube_fw_f4_V1240.zip not installing correctly

I've tried 10 or more times now to get around this problem.I'm choosing the STM32F413RGtx for the uC in STM32CubeIDE new STM32 project,I go to generate code from the embedded CubeMX screen and it always tries to download that stm32cube_fw_f4_v1240.zi...

FStra.9 by Associate III
  • 5403 Views
  • 11 replies
  • 0 kudos

X CUBE AWS STM32 Discovery kit - IoT node

Hello, I'm trying to compile the firmware to use the B-L475E-IOT01A in AWS IoT.I just download the pack X CUBE AWS, import to STM32CubeIDE(v1.0.0 and v1.1.0) and compile.There are two error on make file.I try to make the samething with SW4STM32(v2.9 ...

lenonrt by Associate III
  • 1359 Views
  • 2 replies
  • 0 kudos

Cube IDE Compiler error2

Hi,I'm trying to compile one of AWS project for L475 IoT and I have the silly error: make[1]: *** [vendors/st/stm32l475_discovery/BSP/B-L475E-IOT01/subdir.mk:39: vendors/st/stm32l475_discovery/BSP/B-L475E-IOT01/stm32l475e_iot01.o] Error 2   make: ***...

Tytan28 by Associate
  • 2207 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.