2019-05-27 2:27 AM
Hello,
I created project in TrueStudio for STM32. Now I installed STM32Cube IDE.
I imported my project into STM32Cube IDE. During building this project appeared error:
Error: Program "make" not found in PATH
What is wrong ?
Peter
2019-05-27 5:35 AM
That error is usually due to the project being imported in an unintended way, usually it's because the import requires you to select the "File -> Open projects from file system" choice. Have you followed the migration guide (UM2578)?
I've also seen this when the project were using filters in "Project Properties -> Resource -> Resource Filters" and the project filtered out important files causing import problems as well.
2019-05-30 11:49 PM
2019-06-03 1:37 AM
Can you send the project conversion log to me? It's located in the project root folder and named "PROJECTNAME_converter.log"
2019-06-03 6:02 AM
2019-06-11 1:00 AM
Hi Markus
This is my converter.log:
Post-build step might need some manual actions.
Unknown value type "" for id com.atollic.truestudio.as.general.incpath on tool com.atollic.truestudio.exe.debug.toolchain.as
Unknown value type "" for id com.atollic.truestudio.gcc.symbols.defined on tool com.atollic.truestudio.exe.debug.toolchain.as
Unknown value type "" for id com.atollic.truestudio.common_options.target.interwork on tool com.atollic.truestudio.exe.debug.toolchain.as
Option com.atollic.truestudio.common_options.target.endianess is no longer supported
Option com.atollic.truestudio.common_options.target.instr_set is no longer supported
Unknown value type "" for id com.atollic.truestudio.common_options.target.interwork on tool com.atollic.truestudio.exe.debug.toolchain.gcc
Option com.atollic.truestudio.common_options.target.endianess is no longer supported
Option com.atollic.truestudio.common_options.target.instr_set is no longer supported
Unknown value type "" for id com.atollic.truestudio.ld.libraries.list on tool com.atollic.truestudio.exe.debug.toolchain.ld
Unknown value type "" for id com.atollic.truestudio.ld.libraries.searchpath on tool com.atollic.truestudio.exe.debug.toolchain.ld
Unknown value type "" for id com.atollic.truestudio.common_options.target.interwork on tool com.atollic.truestudio.exe.debug.toolchain.ld
Option com.atollic.truestudio.common_options.target.endianess is no longer supported
Option com.atollic.truestudio.common_options.target.instr_set is no longer supported
Unknown value type "" for id com.atollic.truestudio.gpp.optimization.fno_rtti on tool com.atollic.truestudio.exe.debug.toolchain.gpp
Unknown value type "" for id com.atollic.truestudio.gpp.optimization.fno_exceptions on tool com.atollic.truestudio.exe.debug.toolchain.gpp
Unknown value type "" for id com.atollic.truestudio.common_options.target.interwork on tool com.atollic.truestudio.exe.debug.toolchain.gpp
Option com.atollic.truestudio.common_options.target.endianess is no longer supported
Option com.atollic.truestudio.common_options.target.instr_set is no longer supported
Unknown value type "" for id com.atollic.truestudio.common_options.target.interwork on tool com.atollic.truestudio.exe.debug.toolchain.ldcc
Option com.atollic.truestudio.common_options.target.endianess is no longer supported
Option com.atollic.truestudio.common_options.target.instr_set is no longer supported
No map found for id: com.atollic.truestudio.exe.release
Peter
2019-06-18 11:54 AM
I have a similar problem, i followed the manual too, and when i click on finish nothing happens.
But when i try to open an atollic project in desktop (another directory that does not have workspace) everything works fine in the import proccess, but the project it isn't in workspace.
Anyway, i try to compile to get the .hex and .bin but this happens:
collect2.exe: error: ld returned 1 exit status
make: *** [makefile:58: MyProject.elf] Error 1
"make all" terminated with exit code 2. Build might be incomplete.
And this is my converter log:
Project: MyProject
Converter: Atollic TrueSTUDIO project converter
Date: 20190618
Post-build step might need some manual actions.
Warning: MCU STM32L433RC matched multiple possible MCUs: [STM32L433RCIx, STM32L433RCTx, STM32L433RCTxP, STM32L433RCYx]
Unknown value type "" for id com.atollic.truestudio.gcc.symbols.defined on tool com.atollic.truestudio.exe.debug.toolchain.as
Option com.atollic.truestudio.common_options.target.endianess is no longer supported
Option com.atollic.truestudio.common_options.target.instr_set is no longer supported
Unknown value type "" for id com.atollic.truestudio.common_options.target.interwork on tool com.atollic.truestudio.exe.debug.toolchain.gcc
Option com.atollic.truestudio.common_options.target.endianess is no longer supported
Option com.atollic.truestudio.common_options.target.instr_set is no longer supported
Option com.atollic.truestudio.common_options.target.endianess is no longer supported
Option com.atollic.truestudio.common_options.target.instr_set is no longer supported
No map found for id: com.atollic.truestudio.ld.optimization.malloc_page_size
Unknown value type "" for id com.atollic.truestudio.gpp.optimization.fno_rtti on tool com.atollic.truestudio.exe.debug.toolchain.gpp
Unknown value type "" for id com.atollic.truestudio.gpp.optimization.fno_exceptions on tool com.atollic.truestudio.exe.debug.toolchain.gpp
Option com.atollic.truestudio.common_options.target.endianess is no longer supported
Option com.atollic.truestudio.common_options.target.instr_set is no longer supported
Option com.atollic.truestudio.common_options.target.endianess is no longer supported
Option com.atollic.truestudio.common_options.target.instr_set is no longer supported
No map found for id: com.atollic.truestudio.exe.release
2019-11-01 10:31 PM
Similar importing problem here, running under Ubuntu 18.04
Copied a project that works perfectly under TrueSTUDIO into a new directory that is selected as the STM32CubeIDE working directory.
Followed the migration guide.
The project converter gives 'Fail create backup of project files before conversion'
The project appears to be there but fails to build with no make file - so clearly hasn't migrated properly.
The converter log just says:
Project: LRWAN_V111_AcSIP_Multi_II
Converter: ST System Workbench for STM32 project converter
Date: 20180131
Nothing else.
Tried deleting and starting again. Same issue.
What could be the problem?
Note that the project was originally an STM4SW32 project converted to work with TrueSTUDIO.
Assistance would be appreciated.
Thanks, Ron
2019-11-02 2:59 PM
Found the problem!
There were residual files: .cproject_org, .project_org, and LRWAN_V111_AcSIP_Multi_II_converter.log (LRWAN_V111_AcSIP_Multi_II is the project name) in the project to be converted from a previous conversion from SW4STM32 to TrueSTUDIO
When these files were removed the project imported into STM32CubeIDE ok.
Clearly the import application was failing on trying to write backups to these same file names before importing.
The application would be a bit more robust if an overwrite option was included rather than just giving up without even logging the problem (although of course the log file itself would have had to be overwritten).
2019-11-03 2:01 PM
@Peko , @Markus GIRDLAND what was the resolution?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.