STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Can't use C++ linked to Cube Code generation

I am writing C++ projects using STMCubeIDE and running into a problem when using classes or other C++ features.Even when choosing that the project be a C++ project, I can't build the code. Manually changing the file extensions to .cpp makes the code ...

JKahn.1 by Associate III
  • 1750 Views
  • 2 replies
  • 0 kudos

Where are downloaded mcu packages ?

Hello,I generated a project with the boad wizard. It actually downloaded a big MCU package. I wonder where this is downloaded and if I can find the corresponding HAL and Low-layer drivers documentation.I am on Linux.Thanks

0690X00000DBkFpQAL.png
MRech.1 by Associate II
  • 2199 Views
  • 4 replies
  • 0 kudos

Unable to get a working Blinky

Folks, I have fallen at the first hurdle. I bought a Nucleo-H743Z12, and when it arrived, I checked the jumpers according to the instructions, and plugged it into USB. It lit up its LEDs and performed as expected : The Usr button changed the LED disp...

MEwen.1 by Associate II
  • 3029 Views
  • 6 replies
  • 0 kudos

Resolved! How to set up debugging for Neucleo-64 board in STM32CubeIDE?

I need some assistance in setting up a valid debugging environment in STM32CubeIDE using a Neucleo-64 STM32F103RB board.I have wide experience in C, C++, and C#. I have also experience in the Arduino IDE, having made several projects there. After my ...

SRogers by Associate II
  • 6845 Views
  • 7 replies
  • 0 kudos

Is STM32CubeIDE a tool chain? If so why does everyone including STM recommend some other tool chain in their tutorials? Can anyone recommend a good tutorial or other training source for STM32 programming?

I am in the steepest part of the learning curve for C programming and am experiencing typical frustrations. I can't get "Hello World" to run at this point. I appreciate your patience. I have just ordered the Ritchie Kerighan book and another on STM32...

SGill.1 by Associate II
  • 2737 Views
  • 5 replies
  • 0 kudos

Resolved! CMSIS RTOS V1 Semaphore issues in STM32CubeIDE

Hi,I am using STM32F405, CMSIS RTOS V1, and STM32CubeIDE. I want to create a timer interrupt that periodically release the semaphore to signal the execution of a task. The issue is that it gets stuck after osSemaphoreRelease is called in the interrup...

DLim.16 by Associate II
  • 4267 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.