STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Hello, I was using Atollic studio and I just migrated to STM32CubeIDE, I converted my project initially based to STM32F072CBT6

When STM32CubeIDE started it propose me to select between STM32F072C8Tx or STM32F072C8Ux ...only these choice nothing more. I took the first one, telling to myself that I can change that after.But I cannot the MCU setting is greyed and fix to STM32F0...

[SOLVED] SIMULINK compilation successful but how to continue within STM32CubeIDE and deploy to the board? Some files appear to be missing

Hi everyone,I have bought a STM32F4-Discovery Board DTM32F429I-Disc1, and my intention is to work in Matlab-Simulink.This is the process I have followed:INSTALLATION:Matlab/Simulink R2018b 64bit with toolboxes like Embedded CoderMatlab/Simulink HW su...

DCagi.1 by Associate II
  • 13264 Views
  • 14 replies
  • 0 kudos

STM32CubeIDE 1.2.0 how to debug FreeRTOS multithreading

Hi all,I'm developing an application with FreeRTOS and some task. In debug mode I'd like to jump from one to another without any issue. I really don't understand how. When I pause debug, the compiler always stop in the Idle Task. So I really can't de...

AFara.2 by Associate II
  • 851 Views
  • 0 replies
  • 0 kudos

STM32G431 ADC Wont Calibrate and wont work

Hi I am currently working on a project where I have to use single channel ADC with continuous conversion mode of STM32G431KB on NUCLEO board. However my code stucks at while loop where calibration needs to happen. Also I noticed that ADC12_Common reg...

LLOLO.1 by Associate II
  • 2359 Views
  • 4 replies
  • 0 kudos

Bug with "STM32 Project from STM32CubeMX .ioc file"

Being able to create a new project from an existing .ioc file is very useful. But when I've tried to do this (by selecting File->New->STM32 Project from STM32CubeMX .ioc file) the project seems broken. I can build it fine, but when I try to add new (...

0693W000000UwDDQA0.png

How to copy project from STM32cubeide?

I am using STM32cubeide 1.3.0, and I am running a project called 'test_1'. I want to create a 'test_2' project based on the 'test_1' project, what should I do? I've tried several methods, but I got an error.I tried changing the name of the 'test_1' p...

Snam.1 by Associate
  • 732 Views
  • 0 replies
  • 0 kudos

Bug Creating USART2, USART3 ..... under LL

Hi when I create the USART2 and USART3 under LL using DMA the fieldGPIO_InitStruct.Mode = LL_GPIO_MODE_FLOATING;and will beGPIO_InitStruct.Mode = LL_GPIO_MODE_INPUT;the USART1 work finethanks

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.