STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Does Cube-IDE support launching executables that aren't ELF?

An oldie but still needed, CRC in the last word of the FLASH segment. So I'm fine up until I get to the point when I tell TrueStudio my application is other than an .ELF because at Properties / Run/Debug Settings/ Edit / TrueStudio is hobbled by supp...

n2wx by Senior
  • 7849 Views
  • 16 replies
  • 0 kudos

Enable the UART2 Peripheral Clock

Hello, I am doing a UART example and I need to find the command to Enable the UART2 Peripheral Clock. I have enabled the GPIO clock: __HAL_RCC_GPIOA_CLK_ENABLE(); // stm32f4xx_hal_rcc.hand now I need to enable the UART2 Clock Peripheral. Can anyone ...

JLIND.1 by Associate III
  • 5118 Views
  • 8 replies
  • 0 kudos

FreetRTOS Help

Hello, I am going through a Udemy course on the FreeRTOS. The course does not use the latest version of STM32CubeIDE so I am having some troubles. I am using the Nucleo-F446RE Development kit. I have added the library STM32F4xx_StdPeriph_Driver and t...

JLIND.1 by Associate III
  • 2478 Views
  • 4 replies
  • 0 kudos

code gets lost upon debug

I downloaded the STM32CubeF7 bundle and extracted it. Then made a new folder under the projects folder of the bundle and started STM32CubeIDE with the workspace pointing to the projects folder. I started a new project blinkled and put the blink code ...

KPort.1 by Associate
  • 1084 Views
  • 1 replies
  • 0 kudos

Resolved! STM32CubeIDE Update not working

I get the following error during update in eclipse.An error occurred while collecting items to be installedsession context was:(profile=STM32CubeIDE, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=).No repository found ...

BelSoft by Associate II
  • 10252 Views
  • 12 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.