STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Fault input for HRTIM is configured as output??

Hi, I am working with the HRTIM in the STM32G474 Nucleo and trying to configure the fault input to reset the outputs.When I see in the GPIO config of the HRTIM in the STM32CubeIDE I see that the fault input pin HRTIM_FLT1 is configured as Alternate ...

DKuro.1 by Associate III
  • 1147 Views
  • 0 replies
  • 0 kudos

Strange bug when updating Cube IDE on Mac to 1.3.1

When I update Cube IDE on my Mac to 1.3.1 using the built in updater, it first seems to work fine, although it keeps displaying V1.3.0. I can continue with my work, but when I leave Cube IDE and launch it again, it crashes, reporting it cannot find s...

herbert by Associate III
  • 3027 Views
  • 6 replies
  • 0 kudos

Do not operate the printf() after reboot

Hello, everyone.I am using STM32H753 and STM32CubeIDE.I tried to use the printf () function, but nothing was displayed at the terminal.After seeing an Internet example, I added the following code to use printf():int _write(int file,char *ptr, int len...

Ekim.1 by Associate II
  • 2511 Views
  • 5 replies
  • 0 kudos

multichannel ADC with DMA reads only 0

For my project, i have to read the PA6 and PB0 pins at the same time on my STML082KZT6. These are the ADC_Inch 6 and 8. I have made a code example on STM32CubeMX for the allocations, however the only readings i get are zero.I have allocated uint32_t ...

JWeij.1 by Associate II
  • 827 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.