STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Can't connect to target after power off (STM32F769I-DISCO)

I have the STM32F769I-DISCO board and just made a simple application that uses usart1 to print some debug messages on the virtual com port (USART1. Everything works fine until I power off the board. When the board is connected to usb cable again the ...

0693W000000WSSgQAO.png
ALevc.1 by Associate III
  • 1536 Views
  • 2 replies
  • 0 kudos

STM32H750 + I2S Full Duplex Master + DMA (TX and RX)

Hello,I managed to get full duplex I2S + DMA working on an STM32F405 with Cube + HAL, however have now switched to an STM32H750 for more processing power.In STM32CubeIDE version 1.3.1, while there is an option to add a DMA stream for TX, there is unf...

PSalm.1 by Associate
  • 2503 Views
  • 2 replies
  • 0 kudos

Fault input for HRTIM is configured as output?

Hi, I am working with the HRTIM in the STM32G474 Nucleo and trying to configure the fault input to reset the outputs.When I see in the GPIO config of the HRTIM in the STM32CubeIDE I see that the fault input pin HRTIM_FLT1 is configured as Alternate F...

DKuro.1 by Associate III
  • 1955 Views
  • 2 replies
  • 0 kudos

SWV Debug Config, please help

HelloI was trying to get SWV trace in STM32 CUBE IDE working but it never works.Originally I thought F303K8 is missing SWO connection so I got a new F411RE board but it sill won't work. Can someone help me please? Many thanks!!My Board: F411RE @100Mh...

JHuan.3 by Associate
  • 1411 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.