STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Including 3rd party libraries

Hi, I tried including a few .c and .h files from a 3rd party by dragging and dropping them in the `Inc` and `Src` folders in STM32CubeIDE. However, this did not work and when I tried to build the project, I got a lot of errors on the HAL driver libra...

Debugging Nucleo-F401RE with st-link

I am trying to debug a a nucleo-F401RE with the st-link. About a week ago, it was fine and the code uploaded. I had made it so that the LED on the F401RE turned on and off when I pushed down and released the push button. I came back to it yesterday t...

VZerb.1 by Associate II
  • 7238 Views
  • 11 replies
  • 0 kudos

[STM32F4] Multiple CAN filters using HAL

Good morning,I'm using a CAN bus on my STM32F446RE. Right, now, the CAN communication is working with only one rx filter. I saw in datasheet that we can use up to 128 filters. I don't need so many filters, but I'm trying to configure a second filter....

0693W000006ESbbQAG.png
ValentinG by Associate II
  • 1995 Views
  • 0 replies
  • 0 kudos

Battery management system with stm32F407G and Bare Metal Coding Hello, I would like to design Battery management system

I need just measuring current and voltage of 24 batteriesand accoring to datas, some actions should be taken(stop motor drive,starting of fans vsvsvs)I used,keil microvision,,ATOLLIC true studio, and also Cube IDEBut, I always have problems with libr...

SArsl.1 by Associate II
  • 3447 Views
  • 1 replies
  • 0 kudos

En el Stm32cubeide versión 1.3 existe alguna forma de crear algún proyecto escrito netamente en lenguaje ASM; uso la placa Discovery st.m32f429izt

En el Stm32cubeide versión 1.3 existe alguna forma de crear y escribir algún proyecto netamente en lenguaje ASM; uso la placa Discovery st.m32f429izt; lo que busco es un compilador netamente en ASM que trabaje en el CUBEIDE.Gracias.

LZamb.3 by Associate II
  • 2079 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.