STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32F446 HSE, HSI problem.

Hi guys,I'm facing a problem with STMF446RE MCU. I designed custom stm32f446re board. When i try to upload a program, it uploads successfully but it does not execute it. In STM32CUBEIDE, i can connect a device and achieve debug mode. In debug mode,  ...

GSay.1 by Associate II
  • 2725 Views
  • 6 replies
  • 0 kudos

Resolved! Generate STM32H745I-DISCO (Blinky LED Test)

I have a STM32H745I-DISCO with the STM32CubeIDE platform. I have reviewed various examples that generated the BSP folder for stm32h745i_discovery.h/c files. These files are not generating when creating my own project. I would like to use the BSP_LED_...

DWill.5 by Associate
  • 1695 Views
  • 1 replies
  • 0 kudos

Resolved! How do I import a BSP driver into STMCUBE IDE?

I’m very new to STM32 development so bear with me if this is a simple question. I’m trying to use an L476RG Nucleo and X-Nucleo-ihm03a1 powerSTEP01 board to control stepper motors.I’ve downloaded X-CUBE-SPN3 Driver software expansion for STM32Cube an...

ZHama.1 by Associate II
  • 4390 Views
  • 4 replies
  • 0 kudos

HAL I2C transmit with DMA

I'm stuck trying to transfer a 1024 bit buffer to a SSD1306 via I2C/DMA using the HAL. I am using a stm32L432 nucleo board.Using HAL_I2C_Mem_Write works fine, but HAL_I2C_Mem_Write_DMA only transmits the first 255 bytes and leaves the bus hung on HAL...

Matt R by Associate
  • 998 Views
  • 0 replies
  • 0 kudos

Why does the STM32Cube IDE shows the error "Failed to start GDB server" when debugging/running a simple project for blinking a blue pill's LED

I was going to blink my blue pill (STM32F103C8T6) LED using this tutorial but when hitting the debugger (time 5:50 of the link above) I face the following error:The strange thing is that the IDE recognizes the st link v2 and I can upgrade its firmwar...

0693W000008xxhxQAA.png
Adev.1 by Associate III
  • 842 Views
  • 0 replies
  • 0 kudos

CORDIC EXAMPLE

Hi,I was just looking at an example in STM32 IDE of using CORDIC to calculate SIN and COS. The same is explained in the document below:https://www.st.com/resource/en/application_note/dm00614795-getting-started-with-the-cordic-accelerator-using-stm32c...

MYAQO.1 by Associate II
  • 2514 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.