2021-03-26 12:45 AM
Hi guys,
I'm facing a problem with STMF446RE MCU. I designed custom stm32f446re board. When i try to upload a program, it uploads successfully but it does not execute it. In STM32CUBEIDE, i can connect a device and achieve debug mode. In debug mode, SystemClock_Config(); is freezing but only in HSE. if confg my mcu clock internal resonator HSI, my program works. But in External resonator mode HSE, the SystemClock_Config is freezing in debug mode and program does not execute it. what can be the problem?
Thank you.
2021-03-26 1:23 AM
> is freezing but only in HSE
Your HSE oscillator does not oscillate. Check crystal, check capacitors if they are of proper value, check connections for opens and shorts.
JW
2021-03-26 4:05 AM
I checked them but nothing changes. I also tried different crystals and capacitors but it remain same.
2021-03-26 6:54 AM
Single-step through the code. Where does it exactly "freeze" and how?
Try your code on a "known good" board such as Nucleo or Disco (not necessarily 'F446 - any 'F4 or would do, the clocking scheme is similar).
JW
2021-03-26 7:29 AM
What are you doing with BOOT0 pin? Pulled to ground? VCAP pins? What voltages do you see there?
Write a very small app that just brings up the clocks, perhaps review the RM, and just walk in a couple of interactions with the RCC registers to bring HSE_ON.
Perhaps also route HSE to MCO pin (PA8) so you can measure the the clock without loading the crystal with a scope. Determine if it comes on, how quickly, etc.
2021-03-28 11:52 PM
In void SystemClock_Config(void), i comment out only;
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Configure the main internal regulator output voltage
*/
__HAL_RCC_PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3);
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
and it freeze on last line. I already tried on discovery and it works.
Thanks for your reply.
2021-03-29 12:00 AM
it s pulled to ground and 3.3v i tried both of it one by one and nothing changes. 4.7 uf has been used for Vcap capacitor and there is 1.135v on it. Okay i ll try what you said mate.
Thanks for your reply
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.